This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM335X: Failed to rebuild all after the custom board is added

Part Number: PROCESSOR-SDK-AM335X


I add the custom board(am335x) to SDK according to "3.1.3.6. Creating Board Library with Custom Name" and "3.1.3.7. Creating Custom Board Library for AM335x and AM437x".

It is ok to rebuild board library.C:\ti\pdk_am335x_1_0_17\packages\ti\board>gmake LIMIT_SOCS=am335x LIMIT_BOARDS=myBoard.

But there is two error when rebuild all.(gmake all -j4)

Please help me find the file where the problem is.

Best Regards,

Andy Zhou