Hi TI teams,
we modify LPDDR4 frequency from 4266MTS to 3733MTS,
refer to the link:TDA4VM: how to reduce DDR speed to 3733 MTS - Processors forum - Processors - TI E2E support forums,
but found the board print the error log:

Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI teams,
we modify LPDDR4 frequency from 4266MTS to 3733MTS,
refer to the link:TDA4VM: how to reduce DDR speed to 3733 MTS - Processors forum - Processors - TI E2E support forums,
but found the board print the error log:

Thanks
Hi Sun Ruijie,
The image is not visible, can you please share it again?
Regards,
Brijesh
U-Boot SPL 2021.01-g02bf8f1c2b (Jul 18 2022 - 08:17:20 +0000)
Model: Texas Instruments K3 J721E SoC
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.9.1--v2021.09a (Terrific Lla')
Timeout during frequency handshake
### ERROR ### Please RESET the board ###
resetting ...
Hi Sun,
Which SDK are you on? Did the reverts work correctly? Can you share the steps you did on your setup?
- Keerthy
Hi keerthy,
on 8.2 SDK, the steps is:
cd $PSDKLA_PATH/board-support/u-boot-2021.01+gitAUTOINC+53e79d0e89-g53e79d0e89
git revert 2f21e5b897755334d9a4f2aaacd6945dd2f99cd4
git revert de779d94c7f2b66f0506f44bfc78c2a3e000ecc5
git revert 88f9f21f7ad78a80d1375ee2e7b71ac3ab261b6c
make uboot
Thanks,
Ruijie Sun
Hi,
Followed the exact same steps on 8.2 SDK.
k3conf dump clock 47
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Wed Mar 23 21:04:31 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0016 '22.1.1--v2022.01 (Terrific Llam)') |
|--------------------------------------------------------------------------------|
|---------------------------------------------------------------------------------------|
| Device ID | Clock ID | Clock Name | Status | Clock Frequency |
|---------------------------------------------------------------------------------------|
| 47 | 0 | DEV_DDR0_DDRSS_VBUS_CLK | CLK_STATE_READY | 1000000000 |
| 47 | 1 | DEV_DDR0_PLL_CTRL_CLK | CLK_STATE_READY | 500000000 |
| 47 | 2 | DEV_DDR0_DDRSS_DDR_PLL_CLK | CLK_STATE_READY | 933000000 |
| 47 | 3 | DEV_DDR0_DDRSS_CFG_CLK | CLK_STATE_READY | 125000000 |
| 47 | 4 | DEV_DDR0_DDRSS_IO_CK_N | CLK_STATE_READY | 0 |
| 47 | 5 | DEV_DDR0_DDRSS_IO_CK | CLK_STATE_READY | 0 |
|---------------------------------------------------------------------------------------|
DDR clk is 933000000 * 4 = 3733 MTS.
Hope you copied all the binaries to SD card. Please try the above command.
Best Regards,
Keerthy
hi keerthy,
yes,it is right
root@optimus:/# k3conf dump clock 47
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version 0.2-nogit built Tue May 31 07:06:22 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0015 '21.9.1--v2021.09a (Terrific Lla)') |
|--------------------------------------------------------------------------------|
|---------------------------------------------------------------------------------------|
| Device ID | Clock ID | Clock Name | Status | Clock Frequency |
|---------------------------------------------------------------------------------------|
| 47 | 0 | DEV_DDR0_DDRSS_VBUS_CLK | CLK_STATE_READY | 1000000000 |
| 47 | 1 | DEV_DDR0_PLL_CTRL_CLK | CLK_STATE_READY | 500000000 |
| 47 | 2 | DEV_DDR0_DDRSS_DDR_PLL_CLK | CLK_STATE_READY | 933000000 |
| 47 | 3 | DEV_DDR0_DDRSS_CFG_CLK | CLK_STATE_READY | 125000000 |
| 47 | 4 | DEV_DDR0_DDRSS_IO_CK_N | CLK_STATE_READY | 0 |
| 47 | 5 | DEV_DDR0_DDRSS_IO_CK | CLK_STATE_READY | 0 |
|---------------------------------------------------------------------------------------|
Thanks,
Ruijie Sun