This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c5515 fingerprint kit FDK_DEMO compile error

I have C5515 fingerprint development kit. I want to compile the demo code named as FDK_DEMO which comes with the CD. I am trying to compile it with CCS  Version: 4.2.3.00004. I have followed the instructions under C5515 FDK Software User Guide_SPRUH47.pdf.

First, I have tried it with windows vista home premium which has cygwin installed and I got these errors:

cannot find file "C:/Program\" " FDK_DEMO line 0 1305825854103 209

cannot find file "Collaterals/Software/C5515_code_development/FDK_Demo/rts55x.lib" FDK_DEMO line 0 1305825854103 214

cannot find file "Development\" " FDK_DEMO line 0 1305825854103 212

cannot find file "Files/C5515\" " FDK_DEMO line 0 1305825854103 210

cannot find file "Fingerprint\" " FDK_DEMO line 0 1305825854103 211

cannot find file "Kit\" " FDK_DEMO line 0 1305825854103 213

errors encountered during linking; "C:/Program Files/C5515 Fingerprint Development Kit Collaterals/Software/C5515_code_development/FDK_Demo/Debug/demo.out" not built FDK_DEMO line 0 1305825854119 236

....

I realized that there is a problem with the file system paths which probably caused by cygwin. 

Then, I have tried it windows xp pro sp3 machine which has cygwin installed and I got same errors.

Finally, I tried it with a computer which has windows xp pro sp3 (no cygwin installed) and everything works fine.

Then, I removed cygwin from vista machine but I still get same errors. I don't know how I am gonna fix this issue.

Thanks