This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: TDA4 + OpenGL +SDK8.2+ Errors when rendering 3D

Part Number: TDA4VM


TDA4VM: TDA4 +SDK8.2  

Environment: Ti sdk8.2, tda4

question:

When rendering 3D, process terminated or soc restarted based on SDK8.2.

But the same process works well based on SDK8.0.

While process terminated , the system reports the following error.

Process 270373 (SVVPP) terminated SIGSEGV code=1 fltno=11 ip=0000001e174ebf44(/opt/SVVPP/bin/SVVPP@_ZN9rapidjson12GenericValueINS_4UTF8IcEENS_19MemoryPoolAllocatorINS_12CrtAllocatorEEEEC1El+0x00000000000407b4) mapaddr=0000000000128f44. ref=00000802facec0de

While soc restarted , the system reports nothing error .

The following screenshot shows some logs of the runtime

The first part shows that the graph was verified successfully.

The second part shows that soc2 restarted without any error message .

 

 

What is the reason for this?