Hi
I have trouble building the dsk_app example provided with the dsk6713. I managed to run some other example but i have a probleme with this one (i think i have a problem with dsp/bios projects).
When compiling, i have at the first time 160 errors, maybe 50 errors on each 3 c files: dsk_app.c, aic23.c, and eventually dsk_appcfg_c.c. Most of the errors are:
error: identifier ... is not defined. And the whole identifiers which makes error are those defined in tistdtypes.h. I tried to add include this file at the first line of the files: it works: dsk_app.c and aic23.c compile without errors. But the third file is unaccessible, because it is created by th configuration tool.
I don't see how to add this header in the file, i searched in the configuration tool and found nothing. I also checked the .tcf configuration file but found nothing on headers.
So what do i have to do? Can i add the header someway? But moreover why do i have all those errors. I think most of the people who bought the dsk haven't any trouble making the dsk_app running.
Do i have to do anything about the bios thing? I'm not very sure of that... I want to developp my programm picking ideas in this example, but i would like to do it without bios.
Does the bios brings anything else more than for the debug? I'm not sure to have understood what bios brings compared to csl alone? (i was to do a csl_only project)...
Sorry for all the questions, i've been recently introduced to dsp... I hope someone will be able to help me.
François.