This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ERROR in OMAP35/AM37? datasheet

Hello.

The datasheet for the OMAP35 and the AM37 means, that the pins CAM_STROBE and MMC1_DAT4 both multiplexed to GPIO126. Is this correct? If yes, then these are the only pins who share the same GPIO.

Best regards

Jürgen

  • Jurgen:

    Yes, you can use gpio_126 from either location in the BGA.  If you use gpio_126 as an input,

    set the unused ball to safe_mode, or one of its alternate pin mux settings other than gpio_126.

    Regards,

    Michael T

    PS: Please mark this post as answered via the Verify Answer button below if you think it answers your question.  Thanks!