Hi,
1. Without the (I/O Exp Dcard or The VC Dcard) capture cards, is it possible to encode a yuv file to
h.264 format using the h264venc component of OMTB tool (very similar to the decode_scale_display.oms)
Also, is there any documents available on the relationship between the various ducati components in OMTB tool.
2.I've not found much examples on the OpenMAX demo side apart from the simple decoder. Is it possible
to get example applications using the various ducati components through the Openmax IL library ?
Thanks,
Ganesh.