This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS64GPEVM: Generate and program binary file

Part Number: TMDS64GPEVM


Hi,

i'm using the TMDS64GPEVM evaluation board with the following SDK : mcu_plus_sdk_am64x_08_03_00_18.

Regarding the "Ethernet IP industrial comms example" i've been able to make it run in debug mode and to try it.

Now i'd like to generate the binary file and to flash it to make it run without Code Composer. Which utility and which procedure should i follow to make it?

I'm using, as boot configuration, the following one [OSPI BOOT MODE] :

0 - 7  : ON   - ON - OFF - OFF - ON  - ON  - ON   - OFF

8 - 15 : OFF- ON - OFF - OFF - OFF- OFF- OFF- OFF

Thank you and best regards

Andrea