Part Number: PROCESSOR-SDK-AM62X
Hello,
I try to build the make a tisdk base image and the image run without probleme on am62x_evm board.
If I set the rootfs in read only, by adding in the local.conf the line :
# Set ROOTFS as read-only filesystem
IMAGE_FEATURES += "read-only-rootfs"
The image boot failed during kernel boot, here is the log trace:
[ 0.000000] Reserved memory: created DMA memory pool at 0x000000009cc00000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node m4f-memory@9cc00000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x000000009db00000, size 12 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@9db00000, compatible id shared-dma-pool
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x000000009cafffff]
[ 0.000000] node 0: [mem 0x000000009cb00000-0x000000009e6fffff]
[ 0.000000] node 0: [mem 0x000000009e700000-0x000000009e77ffff]
[ 0.000000] node 0: [mem 0x000000009e780000-0x000000009fffffff]
[ 0.000000] node 0: [mem 0x00000000a0000000-0x00000000ffffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] On node 0 totalpages: 524288
[ 0.000000] DMA zone: 8192 pages used for memmap
[ 0.000000] DMA zone: 0 pages reserved
[ 0.000000] DMA zone: 524288 pages, LIFO batch:63
[ 0.000000] cma: Reserved 144 MiB at 0x00000000f4000000
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.2
[ 0.000000] percpu: Embedded 18 pages/cpu s34752 r8192 d30784 u73728
[ 0.000000] pcpu-alloc: s34752 r8192 d30784 u73728 alloc=18*4096
[ 0.000000] pcpu-alloc: [0] 0 [0] 1 [0] 2 [0] 3
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: ARM erratum 845719
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 516096
[ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 root=PARTUUID=8b7cbc72-02 rw rootfstype=ext4 rootwait
[ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] Memory: 1836952K/2097152K available (10688K kernel code, 1166K rwdata, 4156K rodata, 1728K init, 436K bss, 112744K reserved, 147456K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
[ 0.000000] rcu: RCU priority boosting: priority 1 delay 500 ms.
[ 0.000000] rcu: RCU_SOFTIRQ processing moved to rcuc kthreads.
[ 0.000000] No expedited grace period (rcu_normal_after_boot).
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 256 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] GICv3: Distributor has no Range Selector support
[ 0.000000] GICv3: 16 PPIs implemented
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000
[ 0.000000] ITS [mem 0x01820000-0x0182ffff]
[ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[ 0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
[ 0.000000] ITS@0x0000000001820000: allocated 524288 Devices @80800000 (flat, esz 8, psz 64K, shr 0)
[ 0.000000] ITS: using cache flushing for cmd queue
[ 0.000000] GICv3: using LPI property table @0x0000000080040000
[ 0.000000] GIC: using cache flushing for LPI property table
[ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000080050000
[ 0.000000] random: get_random_bytes called from start_kernel+0x320/0x4c8 with crng_init=0
[ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[ 0.000001] sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[ 0.008467] Console: colour dummy device 80x25
[ 0.013064] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[ 0.023745] pid_max: default: 32768 minimum: 301
[ 0.028563] LSM: Security Framework initializing
[ 0.033348] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.040930] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.050795] rcu: Hierarchical SRCU implementation.
[ 0.056215] Platform MSI: msi-controller@1820000 domain created
[ 0.062558] PCI/MSI: /bus@f0000/interrupt-controller@1800000/msi-controller@1820000 domain created
[ 0.071837] EFI services will not be available.
[ 0.076763] smp: Bringing up secondary CPUs ...
[ 0.092741] Detected VIPT I-cache on CPU1
[ 0.096875] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000
[ 0.103914] GICv3: CPU1: using allocated LPI pending table @0x0000000080060000
[ 0.111353] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.129519] Detected VIPT I-cache on CPU2
[ 0.133649] GICv3: CPU2: found redistributor 2 region 0:0x00000000018c0000
[ 0.140684] GICv3: CPU2: using allocated LPI pending table @0x0000000080070000
[ 0.148104] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[ 0.166141] Detected VIPT I-cache on CPU3
[ 0.170264] GICv3: CPU3: found redistributor 3 region 0:0x00000000018e0000
[ 0.177298] GICv3: CPU3: using allocated LPI pending table @0x0000000080080000
[ 0.184712] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[ 0.191483] smp: Brought up 1 node, 4 CPUs
[ 0.195689] SMP: Total of 4 processors activated.
[ 0.200509] CPU features: detected: 32-bit EL0 Support
[ 0.205771] CPU features: detected: CRC32 instructions
[ 0.218236] CPU: All CPU(s) started at EL2
[ 0.222447] alternatives: patching kernel code
[ 0.228221] devtmpfs: initialized
[ 0.238710] KASLR disabled due to lack of seed
[ 0.243478] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.253458] futex hash table entries: 1024 (order: 5, 131072 bytes, linear)
[ 0.265148] pinctrl core: initialized pinctrl subsystem
[ 0.271162] DMI not present or invalid.
[ 0.275646] NET: Registered protocol family 16
[ 0.282426] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
[ 0.289807] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.297925] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.306735] thermal_sys: Registered thermal governor 'step_wise'
[ 0.307169] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.320354] ASID allocator initialised with 65536 entries
[ 0.350654] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.357568] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.364462] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.371325] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.379205] cryptd: max_cpu_qlen set to 1000
[ 0.386632] k3-chipinfo 43000014.chipid: Family:AM62X rev:SR1.0 JTAGID[0x0bb7e02f] Detected
[ 0.395787] vcc_5v0: supplied by vmain_pd
[ 0.400351] vcc_3v3_sys: supplied by vmain_pd
[ 0.405437] vcc_1v8: supplied by vcc_3v3_sys
[ 0.410857] iommu: Default domain type: Translated
[ 0.416263] SCSI subsystem initialized
[ 0.420552] mc: Linux media interface: v0.10
[ 0.424971] videodev: Linux video capture interface: v2.00
[ 0.430678] pps_core: LinuxPPS API ver. 1 registered
[ 0.435766] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.445125] PTP clock support registered
[ 0.449166] EDAC MC: Ver: 3.0.0
[ 0.453051] omap-mailbox 29000000.mailbox: omap mailbox rev 0x66fc9100
[ 0.460236] FPGA manager framework
[ 0.463836] Advanced Linux Sound Architecture Driver Initialized.
[ 0.471051] clocksource: Switched to clocksource arch_sys_counter
[ 0.477533] VFS: Disk quotas dquot_6.6.0
[ 0.481610] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.495206] NET: Registered protocol family 2
[ 0.499918] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.508739] tcp_listen_portaddr_hash hash table entries: 1024 (order: 4, 65536 bytes, linear)
[ 0.517552] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
[ 0.525808] TCP bind hash table entries: 16384 (order: 7, 917504 bytes, linear)
[ 0.534215] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.541329] UDP hash table entries: 1024 (order: 5, 131072 bytes, linear)
[ 0.548451] UDP-Lite hash table entries: 1024 (order: 5, 131072 bytes, linear)
[ 0.556238] NET: Registered protocol family 1
[ 0.561352] RPC: Registered named UNIX socket transport module.
[ 0.567456] RPC: Registered udp transport module.
[ 0.572267] RPC: Registered tcp transport module.
[ 0.577076] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.583672] PCI: CLS 0 bytes, default 64
[ 0.588631] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
[ 0.600881] Initialise system trusted keyrings
[ 0.605666] workingset: timestamp_bits=46 max_order=19 bucket_order=0
[ 0.617511] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.624216] NFS: Registering the id_resolver key type
[ 0.629447] Key type id_resolver registered
[ 0.633735] Key type id_legacy registered
[ 0.637935] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.644807] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 0.652694] 9p: Installing v9fs 9p2000 file system support
[ 0.694486] Key type asymmetric registered
[ 0.698714] Asymmetric key parser 'x509' registered
[ 0.703817] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
[ 0.711394] io scheduler mq-deadline registered
[ 0.716048] io scheduler kyber registered
[ 0.722150] pinctrl-single 4084000.pinctrl: 34 pins, size 136
[ 0.728566] pinctrl-single f4000.pinctrl: 171 pins, size 684
[ 0.742232] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 0.763711] brd: module loaded
[ 0.776484] loop: module loaded
[ 0.780513] megasas: 07.714.04.00-rc1
[ 0.788327] tun: Universal TUN/TAP device driver, 1.6
[ 0.794075] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[ 0.800519] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 0.806652] sky2: driver version 1.30
[ 0.811359] VFIO - User Level meta-driver version: 0.3
[ 0.817723] i2c /dev entries driver
[ 0.822226] sdhci: Secure Digital Host Controller Interface driver
[ 0.828573] sdhci: Copyright(c) Pierre Ossman
[ 0.833324] sdhci-pltfm: SDHCI platform and OF driver helper
[ 0.840388] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 0.848261] optee: probing for conduit method.
[ 0.852869] optee: revision 3.12 (3d47a131)
[ 0.853409] optee: initialized driver
[ 0.863546] NET: Registered protocol family 17
[ 0.868305] 9pnet: Installing 9P2000 support
[ 0.872755] Key type dns_resolver registered
[ 0.877495] printk: bootconsole [ns16550a0]: printing thread started
[ 0.877544] Loading compiled-in X.509 certificates
[ 0.888636] ti-sci 44043000.system-controller: ti,ctx-memory-region is required for suspend but not provided.
[ 0.888654] ti-sci 44043000.system-controller: ti_sci_init_suspend failed, mem suspend will be non-functional.
[ 0.888661] ti-sci 44043000.system-controller: ABI: 3.1 (firmware rev 0x0008 '8.3.2--v08.03.02 (Jolly Jellyfi')
[ 1.415066] davinci-mcasp 2b10000.mcasp: IRQ common not found
[ 1.464478] omap_i2c 20000000.i2c: bus 0 rev0.12 at 400 kHz
[ 1.475818] omap_i2c 20010000.i2c: bus 1 rev0.12 at 100 kHz
[ 1.476439] ti-sci-intr 4210000.interrupt-controller: Interrupt Router 5 domain created
[ H��1.476677] ti-sci-intr bus@f0000:interrupt-controller@a00000: Interrupt Router 3 domain created
[ 1.477053] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created
[ 1.502246] printk: console [ttyS2]: printing thread started
[ 1.477381] ti-bcdma 485c0100.dma-controller: Number of rings: 82
[ 1.502262] printk: console [ttyS2] enabled
[ 1.502266] printk: bootconsole [ns16550a0] disabled
[ 1.522875] printk: bootconsole [ns16550a0]: printing thread stopped
[ 1.570300] spi-nor spi0.0: s28hs512t (65536 Kbytes)
[ 1.570361] 7 fixed-partitions partitions found on MTD device fc40000.spi.0
[ 1.570368] Creating 7 MTD partitions on "fc40000.spi.0":
[ 1.570374] 0x000000000000-0x000000080000 : "ospi.tiboot3"
[ 1.571999] 0x000000080000-0x000000280000 : "ospi.tispl"
[ 1.573341] 0x000000280000-0x000000680000 : "ospi.u-boot"
[ 1.574633] 0x000000680000-0x0000006c0000 : "ospi.env"
[ 1.575991] 0x0000006c0000-0x000000700000 : "ospi.env.backup"
[ 1.577297] 0x000000800000-0x000003fc0000 : "ospi.rootfs"
[ 1.578609] 0x000003fc0000-0x000004000000 : "ospi.phypattern"
[ 1.647100] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 1.650375] davinci_mdio 8000f00.mdio: phy[0]: device 8000f00.mdio:00, driver TI DP83867
[ 1.650393] davinci_mdio 8000f00.mdio: phy[1]: device 8000f00.mdio:01, driver TI DP83867
[ 1.650503] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA01103, cpsw version 0x6BA81103 Ports: 3 quirks:00000002
[ 1.651987] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 19
[ 1.652391] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.5
[ 1.652399] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512
[ 1.658545] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:0
[ 1.673729] rtc-ti-k3 2b1f0000.rtc: registered as rtc0
[ 1.673770] rtc-ti-k3 2b1f0000.rtc: setting system clock to 1970-01-01T00:00:08 UTC (8)
[ 1.717892] davinci-mcasp 2b10000.mcasp: IRQ common not found
[ 1.771635] mmc0: CQHCI version 5.10
[ 1.812957] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit
[ 1.859757] reg-fixed-voltage regulator-6: Failed to register regulator: -517
[ 1.860642] pca953x 1-0022: supply vcc not found, using dummy regulator
[ 1.860780] pca953x 1-0022: using AI
[ 1.886607] sii902x 1-003b: supply iovcc not found, using dummy regulator
[ 1.886754] sii902x 1-003b: supply cvcc12 not found, using dummy regulator
[ 1.889413] i2c i2c-1: Added multiplexed i2c bus 2
[ 1.954953] [drm] Initialized tidss 1.0.0 20180215 for 30200000.dss on minor 0
[ 2.071935] Console: switching to colour frame buffer device 240x75
[ 2.103692] tidss 30200000.dss: [drm] fb0: tidssdrmfb frame buffer device
[ 2.113842] vdd_mmc1: supplied by vcc_3v3_sys
[ 2.115889] wlan_lten: supplied by vcc_3v3_sys
[ 2.116716] wlan_en: supplied by wlan_lten
[ 2.117936] debugfs: Directory 'pd:182' with parent 'pm_genpd' already present!
[ 2.333813] ALSA device list:
[ 2.333830] No soundcards found.
[ 2.340002] mmc2: CQHCI version 5.10
[ 2.350311] mmc1: CQHCI version 5.10
[ 2.381766] mmc2: SDHCI controller on fa20000.mmc [fa20000.mmc] using ADMA 64-bit
[ 2.387803] sdhci-am654 fa20000.mmc: card claims to support voltages below defined range
[ 2.391833] mmc1: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64-bit
[ 2.392387] Waiting for root device PARTUUID=8b7cbc72-02...
[ 2.401081] mmc2: new high speed SDIO card at address 0001
[ 2.426013] mmc1: new high speed SDHC card at address 5048
[ 2.426936] mmcblk1: mmc1:5048 Y032V 28.9 GiB
[ 2.429514] mmcblk1: p1 p2
[ 2.450267] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)
[ 2.450391] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 2.451395] devtmpfs: mounted
[ 2.452998] Freeing unused kernel memory: 1728K
[ 2.475140] Run /sbin/init as init process
[ 2.778317] systemd[1]: System time before build time, advancing clock.
[ 2.872638] NET: Registered protocol family 10
[ 2.874081] Segment Routing with IPv6
[ 2.910939] systemd[1]: systemd 244.5+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLK)
[ 2.911763] systemd[1]: Detected architecture arm64.
Welcome to Arago 2021.09!
[ 2.956632] systemd[1]: Set hostname to <am62xx-evm>.
[ 3.413378] random: systemd: uninitialized urandom read (16 bytes read)
[ 3.413745] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling.
[ 3.413761] systemd[1]: (This warning is only shown for the first unit using IP firewalling.)
[ 3.417716] systemd[1]: Created slice system-getty.slice.
[ OK ] Created slice system-getty.slice.
[ OK ] Created slice system-serial\x2dgett[ 3.463371] random: systemd: uninitialized urandom read (16 bytes read)
y.slice.
[ 3.465086] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ 3.485321] random: systemd: uninitialized urandom read (16 bytes read)
[ 3.486916] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ OK ] Started Dispatch Password �…ts to [ 3.515765] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
Console Directory Watch.
[ OK ] Started Forward Password R�…uests [ 3.539607] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
to Wall Directory Watch.
[ OK ] Reached target Paths.
[ 3.563527] systemd[1]: Reached target Paths.
[ OK ] Reached target Remote File Systems 3.575330] systemd[1]: Reached target Remote File Systems.
[0m.
[ OK ] Reached target Slices.
[ 3.595283] systemd[1]: Reached target Slices.
[ OK ] Reached target Swap.
[ 3.607288] systemd[1]: Reached target Swap.
[ OK ] Listening on RPCbind Server Activat[ 3.660299] systemd[1]: Listening on RPCbind Server Activation Socket.
ion Socket.
[ OK ] Reached target RPC Port Mapper.[ 3.683418] systemd[1]: Reached target RPC Port Mapper.
[ OK ] Listening on Process Core Dump Sock[ 3.709350] systemd[1]: Listening on Process Core Dump Socket.
et.
[ OK ] Listening on initctl Compatibility [ 3.731839] systemd[1]: Listening on initctl Compatibility Named Pipe.
Named Pipe.
[ OK ] Listening on Journal Socket (/dev/l[ 3.771707] systemd[1]: Condition check resulted in Journal Audit Socket being skipped.
og).
[ 3.772829] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket.
[ 3.794610] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Network Service Netlin[ 3.808355] systemd[1]: Listening on Network Service Netlink Socket.
k Socket.
[ OK ] Listening on udev Control Socket 3.832168] systemd[1]: Listening on udev Control Socket.
m.
[ OK ] Listening on udev Kernel Socket[ 3.855853] systemd[1]: Listening on udev Kernel Socket.
.
Mounting Huge Pages File System...[ 3.885822] systemd[1]: Mounting Huge Pages File System...
Mounting POSIX Message Queue File System..[ 3.913317] systemd[1]: Mounting POSIX Message Queue File System...
.
Mounting Kernel Debug File System...[ 3.947953] systemd[1]: Mounting Kernel Debug File System...
Mounting Temporary Directory (/tmp)...
[ 3.977919] systemd[1]: Mounting Temporary Directory (/tmp)...
Starting Create list of st�…odes for the curr[ 3.996221] systemd[1]: Starting Create list of static device nodes for the current kernel...
ent kernel...
Starting Start psplash boot splash screen.[ 4.024971] systemd[1]: Starting Start psplash boot splash screen...
..
[ 4.054955] systemd[1]: Starting RPC Bind...
Starting RPC Bind...
Starting Journal Service...[ 4.118465] systemd[1]: Starting Journal Service...
Starting Load Kernel Modules...[ 4.148974] systemd[1]: Starting Load Kernel Modules...
[ 4.174818] cryptodev: loading out-of-tree module taints kernel.
Starting Remount Root and Kernel File Systems 4.179828] systemd[1]: Starting Remount Root and Kernel File Systems...
[0m...
[ 4.181599] cryptodev: driver 1.10 loaded.
Starting udev Coldplug all Devices...
[ 4.213035] systemd[1]: Starting udev Coldplug all Devices...
[ OK ] Started RPC Bind.
[ 4.237935] systemd[1]: Started RPC Bind.
[ OK ] Started Start psplash boot splash s[ 4.248588] systemd[1]: Started Start psplash boot splash screen.
creen.
[ 4.270738] EXT4-fs (mmcblk1p2): re-mounted. Opts: (null)
[ OK ] Started Journal Service.
[ 4.281315] systemd[1]: Started Journal Service.
[ OK ] Mounted Huge Pages File System.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Mounted Kernel Debug File System.
[ OK ] Mounted Temporary Directory (/tmp).
[ OK ] Started Create list of sta�… nodes for the current kernel.
[ OK ] Started Load Kernel Modules.
[ OK ] Started Remount Root and Kernel File Systems.
Mounting Kernel Configuration File System...
[ OK ] Started Start psplash-syst�…progress communication helper.
Starting Flush Journal to Persistent Storage...
[ 4.511930] systemd-journald[215]: Received client request to flush runtime journal.
Starting Apply Kernel Variables...
Starting Create Static Device Nodes in /dev...
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Started Apply Kernel Variables.
[ OK ] Started Create Static Device Nodes in /dev.
[ OK ] Reached target Local File Systems (Pre).
Mounting /media/ram...
Mounting /var/volatile...
Starting udev Kernel Device Manager...
[FAILED] Failed to mount /media/ram.
See 'systemctl status media-ram.mount' for details.
[DEPEND] Dependency failed for Local File Systems.
[ OK ] Mounted /var/volatile.
[ OK ] Stopped Dispatch Password �…ts to Console Directory Watch.
[ OK ] Stopped Forward Password R�…uests to Wall Directory Watch.
[ OK ] Reached target Timers.
[ OK ] Reached target Network (Pre).
[ OK ] Reached target Login Prompts.
Starting Synchronize System and HW clocks...
Starting Bind mount volatile /var/cache...
Starting Bind mount volatile /var/lib...
[ 5.515965] overlayfs: upper fs does not support xattr, falling back to index=off and metacopy=off.
[ 5.522010] overlayfs: upper fs does not support xattr, falling back to index=off and metacopy=off.
Starting Bind mount volatile /var/spool...
[ OK ] Reached target Sockets.
[ 5.618112] overlayfs: upper fs does not support xattr, falling back to index=off and metacopy=off.
[ OK ] Started Emergency Shell.
[ OK ] Reached target Emergency Mode.
Starting Create Volatile Files and Directories...
[ OK ] Started udev Kernel Device Manager.
[ OK ] Started udev Coldplug all Devices 5.803529] CAN device driver interface
0m.
[ OK ] Started Synchronize System and HW c[ 5.855866] m_can_platform 20701000.can: m_can device registered (irq=34, version=32)
locks.
[ OK ] Started Bind mount volatile /var/cache.
[ OK ] Started Bind mount volatile /var/lib.
[ OK ] Started Bind mount volatile /var/spool.
[ OK ] Started Create Volatile Files and Directories.
[ 6.372491] k3-m4-rproc 5000000.m4fss: assigned reserved memory node m4f-dma-memory@9cb00000
[ 6.372863] k3-m4-rproc 5000000.m4fss: configured M4 for remoteproc mode
[ 6.387149] k3-m4-rproc 5000000.m4fss: local reset is deasserted for device
[ 6.423404] remoteproc remoteproc0: 5000000.m4fss is available
[ 6.425013] remoteproc remoteproc0: Direct firmware load for am62-mcu-m4f0_0-fw failed with error -2
[ 6.425057] remoteproc remoteproc0: powering up 5000000.m4fss
[ 6.425095] remoteproc remoteproc0: Direct firmware load for am62-mcu-m4f0_0-fw failed with error -2
[ 6.425105] remoteproc remoteproc0: request_firmware failed: -2
Starting Network Service...
Starting Load/Save Random Seed...
Starting Network Time Synchronization...
Starting Update UTMP about System Boot/Shutdown...
[ 7.087228] PVR_K: 235: Read BVNC 33.15.11.3 from HW device registers
[ 7.087262] PVR_K: 235: RGX Device registered with BVNC 33.15.11.3
[ OK ] Started Update UTMP about System Bo[ 7.107309] [drm] Initialized pvr 1.15.6133109 20170530 for fd00000.gpu on minor 1
ot/Shutdown.
Starting Update UTMP about System Runlevel Changes...
[ OK ] Started Update UTMP about System Runlevel Changes.
[ OK ] Started Network Service.
Starting Wait for Network to be Configured...
[ 7.483357] TI DP83867 8000f00.mdio:01: attached PHY driver [TI DP83867] (mii_bus:phy_addr=8000f00.mdio:01, irq=POLL)
[ 7.486647] am65-cpsw-nuss 8000000.ethernet eth1: Link is Down
Starting Network Name Resolution...
[ 7.646270] TI DP83867 8000f00.mdio:00: attached PHY driver [TI DP83867] (mii_bus:phy_addr=8000f00.mdio:00, irq=POLL)
[ 7.651147] am65-cpsw-nuss 8000000.ethernet eth0: Link is Down
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Time Set.
[ OK ] Reached target System Time Synchronized.
[ OK ] Started Network Name Resolution.
[ OK ] Reached target Network.
[ OK ] Reached target Host and Network Name Lookups.
[ OK ] Started NFS status monitor for NFSv2/3 locking..
[ 8.875207] random: crng init done
[ 8.875237] random: 7 urandom warning(s) missed due to ratelimiting
[ OK ] Started Load/Save Random Seed.
[ OK ] Created slice system-systemd\x2dfsck.slice.
[ OK ] Found device /dev/disk/by-uuid/5ED4-6015.
[ OK ] Found device /dev/mmcblk1p1.
[ 9.530123] remoteproc remoteproc1: 30074000.pru is available
[ 9.567382] remoteproc remoteproc2: 30078000.pru is available
[ 9.593165] cdns-csi2rx: probe of 30101000.csi-bridge failed with error -22
[ 9.646646] omap_rng 40910000.rng: Random Number Generator ver. 241b34c
Mounting /boot...
Starting File System Check on /dev/mmcblk1p1 9.730681] tps6598x 0-003f: Unable to find the interrupt, switching to polling
0m...
[ 9.801969] usbcore: registered new interface driver usbfs
[ 9.802046] usbcore: registered new interface driver hub
[ 9.802134] usbcore: registered new device driver usb
[ 9.842666] FAT-fs (mmcblk1p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ 9.851987] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ OK ] Mounted /boot.
[ 9.868832] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller
[ 9.868911] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 1
[ 9.869244] xhci-hcd xhci-hcd.2.auto: hcc params 0x0258fe6d hci version 0x110 quirks 0x0000000000010010
[ OK ] Reached target Sound Card.
[ OK ] Reached target Hardware activated U[ 9.869718] xhci-hcd xhci-hcd.2.auto: irq 474, io mem 0x31100000
SB gadget.
[ OK ] Listening on Load/S[ 9.869967] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 9.870271] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[ 9.870301] cfg80211: failed to load regulatory.db
ave RF �…itch Status /dev/rfkill Watch.
[ 9.870335] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.10
[ 9.870345] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 9.870351] usb usb1: Product: xHCI Host Controller
[ 9.870361] usb usb1: Manufacturer: Linux 5.10.109-rt65-gd9ee8a25c2 xhci-hcd
[ 9.870366] usb usb1: SerialNumber: xhci-hcd.2.auto
[ 9.881313] hub 1-0:1.0: USB hub found
[ 9.881401] hub 1-0:1.0: 1 port detected
[ 9.884344] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller
[ 9.884391] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 2
[ OK ] Started File System Check on /dev/m[ 9.884420] xhci-hcd xhci-hcd.2.auto: Host supports USB 3.0 SuperSpeed
mcblk1p1.[ 9.884607] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 9.884750] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 5.10
[ 9.884759] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 9.884766] usb usb2: Product: xHCI Host Controller
[ 9.884773] usb usb2: Manufacturer: Linux 5.10.109-rt65-gd9ee8a25c2 xhci-hcd
[ 9.884779] usb usb2: SerialNumber: xhci-hcd.2.auto
[ 9.885643] hub 2-0:1.0: USB hub found
[ 9.885698] hub 2-0:1.0: config failed, hub doesn't have any ports! (err -19)
Mounting /run/media/mmcblk1p1...
[ OK ] Mounted /run/media/mmcblk1p1.
[ 10.091300] wl18xx_driver wl18xx.1.auto: Direct firmware load for ti-connectivity/wl1271-nvs.bin failed with error -2
[ 10.091374] wl18xx_driver wl18xx.1.auto: Direct firmware load for ti-connectivity/wl18xx-conf.bin failed with error -2
[ 10.091383] wlcore: ERROR could not get configuration binary ti-connectivity/wl18xx-conf.bin: -2
[ 10.091388] wlcore: WARNING falling back to default config
[ 10.135141] usb 1-1: new full-speed USB device number 2 using xhci-hcd
[ 10.285166] usb 1-1: New USB device found, idVendor=046d, idProduct=c52e, bcdDevice=23.01
[ 10.285189] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[ 10.285196] usb 1-1: Product: USB Receiver
[ 10.285201] usb 1-1: Manufacturer: Logitech
[ 10.385389] input: Logitech USB Receiver as /devices/platform/bus@f0000/f910000.dwc3-usb/31100000.usb/xhci-hcd.2.auto/usb1/1-1/1-1:1.0/0003:046D:C52E.0001/input/input0
[ 10.444022] hid-generic 0003:046D:C52E.0001: input: USB HID v1.11 Keyboard [Logitech USB Receiver] on usb-xhci-hcd.2.auto-1/input0
[ 10.451813] input: Logitech USB Receiver Mouse as /devices/platform/bus@f0000/f910000.dwc3-usb/31100000.usb/xhci-hcd.2.auto/usb1/1-1/1-1:1.1/0003:046D:C52E.0002/input/input1
[ 10.452292] input: Logitech USB Receiver Consumer Control as /devices/platform/bus@f0000/f910000.dwc3-usb/31100000.usb/xhci-hcd.2.auto/usb1/1-1/1-1:1.1/0003:046D:C52E.0002/input/inp2
[ 10.501942] wlcore: wl18xx HW: 183x or 180x, PG 2.2 (ROM 0x11)
[ 10.510911] wlcore: loaded
[ 10.517222] input: Logitech USB Receiver System Control as /devices/platform/bus@f0000/f910000.dwc3-usb/31100000.usb/xhci-hcd.2.auto/usb1/1-1/1-1:1.1/0003:046D:C52E.0002/input/input3
Starting Load/Save RF Kill Switch Status..[ 10.519005] hid-generic 0003:046D:C52E.0002: input: USB HID v1.11 Mouse [Logitech USB Receiver] on usb-xhci-hcd.2.auto-1/input1
.
[ 10.520719] usbcore: registered new interface driver usbhid
[ 10.520761] usbhid: USB HID core driver
[ OK ] Started Load/Save RF Kill Switch Status.
You are in emergency mode. After logging in, type "journalctl -xb" to view
system logs, "systemctl reboot" to reboot, "systemctl default" or "exit"
to boot into default mode.
Give root password for maintenance
(or press Control-D to continue): [ 11.131577] wl18xx_driver wl18xx.1.auto: Direct firmware load for ti-connectivity/wl18xx-fw-4.bin failed with error -2
[ 11.131617] wlcore: ERROR could not get firmware ti-connectivity/wl18xx-fw-4.bin: -2
[ 11.515399] wl18xx_driver wl18xx.1.auto: Direct firmware load for ti-connectivity/wl18xx-fw-4.bin failed with error -2
[ 11.515435] wlcore: ERROR could not get firmware ti-connectivity/wl18xx-fw-4.bin: -2
[ 11.899537] wl18xx_driver wl18xx.1.auto: Direct firmware load for ti-connectivity/wl18xx-fw-4.bin failed with error -2
[ 11.899570] wlcore: ERROR could not get firmware ti-connectivity/wl18xx-fw-4.bin: -2
[ 11.899661] wlcore: ERROR firmware boot failed despite 3 retries
Could you tell me what is the proper way to make the rootfs in readonly with for ti sdk ?
Regards,
Alexis.