This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

confusing about LCDC user guide LIDD part

file : SPRUFV5A, august 2010

page 13, table 3 LIDD I/O Name Map

display type :Micro interface  

interface type :8080

LIDD_CTRL[2:0]: 011  

LCD_PCLK                                          RD

LCD_HSYNC:                                      WR

LCD_VSYNC:                                       A0

LCD_AC_ENB_CS                            CS(or CS0)

LCD_MCLK:                                        CS1

 

page 30, table 14. LIDD_CTRL field descriptions

pin                                                       011b

LCD_PCLK                                        RS

LCD_HSYNC                                     WS

LCD_VSYNC                                      ALE

LCD_AC_ENB_CS                           CS0

LCD_MCLK                                        CS1

there must be something wrong with the signal defines, so anybody could give me the timing for each pin's output or make it clear so that I could use it in the right way?

 

regards,

Power Pan