As the title, I want to make sure if TDA4VM DP support YUV422 format output?
We're using 08_02_00_03 linux SDK and 08_02_00_05 RTOS SDK.
Because on chapter 12.6.1.2 of TRM says that "YUV422 planar formats (8-bit and 10-bit) for video pipelines and write-back" not support
But on chapter 1.3.14 of TRM says that "eDP features include YCbCr422(via simple decimation)",
So I'm confuse about this, what formats does TDA4VM DP/eDP supported?
BR,
Shawn