Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to configure example on EB

Other Parts Discussed in Thread: DRA821

Hi team,

Here's an issue from the customer may need your help:

DRA821 is used and as shown in the figure, the customer imported the routine of the mcal library, but did not know how to configure the parameters. So they would like to know is there any related docs for reference.

Could you help check this case? Thanks.

Best Regards,

Cherry

  • Hello,

    We have a guide on how to use the EB Tresos configurator to modify the behavior of the MCAL drivers as part of our MCUSW documentation.

    Please see here: https://software-dl.ti.com/jacinto7/esd/processor-sdk-rtos-jacinto7/latest/exports/docs/mcusw/mcal_drv/docs/drv_docs/mcusw_cfg_ug_top.html

    Are there any specific questions about the configuration being used?

    Regards,

    Erick

  • Hello Erick,

    Thanks for your support.

    Do we have any docs or examples could specify on how a module configures parameters, what each parameter does etc.?

    Thanks and regards,

    Cherry

  • Cherry,

    The configurator usage is described in the docs I linked, you can see how to install tresos, add the plugins for your device and configure them.

    The parameters themselves are mostly defined by the AUTOSAR standard, you can find definitions on them in the AUTOSAR spec. For example, looking at the ADC example above:

    The spec describes what the parameters mean. There may be some TI-defined parameters specific to TI MCAL drivers, those will be defined in the MCUSW documentation.

    Please let me know if you have any more questions.

    Regards,

    Erick

  • Hello, I have finished reading this document, but there is no discussion on how to configure the parameters in the figure. Is there any example on how to configure the parameters in a certain module, the specific function of each parameter, and what kind of configuration to achieve what function

  • Hey Erick,

    Thanks and yang ying is the customer I mentioned and may I know are there any AUTOSAR related docs available?

    Thanks and regards,

    Cherry

  • Hi Yang Ying, Cherry,

    there is no discussion on how to configure the parameters in the figure

    We do not have a guide on changing specific configurations for particular usecases.

    Is there any example on how to configure the parameters in a certain module, the specific function of each parameter, and what kind of configuration to achieve what function

    The configurator ensures that the configuration you make on a driver is valid (there is a Validation button), so you can be sure that the values you chose are OK. There isn't examples of different configurations, the only example is the default configuration that is provided with the Plugin. You can modify the parameters as needed for your usecase. The configurators default values should reflect the one used for the example applications, so you can reference those to see why it was configured this way.

    Is there something you want to enable on the ADC Driver that you need help with?

    are there any AUTOSAR related docs available

    AUTOSAR standard documentation is available on their website: https://www.autosar.org/

    If you mean AUTOSAR provided by a vendor, it would be best to get documentation directly from them as we don't provide an AUTOSAR implementation, just the MCAL.

    Is there specific AUTOSAR documentation you are looking for?

    Regards,

    Erick