Hello,
I'm trying to compiling an app for ARM Cortex R5F core with ti-cgt-armllvm_1.3.0.LTS but got the following error:
$ "/home/mmao/ti/ccs1110/ccs/tools/compiler/ti-cgt-armllvm_1.3.0.LTS/bin/tiarmclang" -std=c11 -mcpu=cortex-r5 -mfloat-abi=hard -mfpu=vfpv3-d16 -m32 -O0 -g3 -pipe -fno-short-enums -fno-builtin -Wno-gnu-variable-sized-type-not-at-end -Wno-unused-function -L _build/TI_ARMLLVM/HSM/lib/ -L "/home/mmao/ti/ccs1110/ccs/tools/compiler/ti-cgt-armllvm_1.3.0.LTS/lib" -o _build/TI_ARMLLVM/TI_ARMLLVM -L _build/TI_ARMLLVM/HSM/bin -L _build/TI_ARMLLVM/HOST/bin -llibHSM.lib -llibHOST_tests.lib -llibHOST.lib -v
TI Arm Clang Compiler 1.3.0.LTS
Target: arm-ti-none-eabi
Thread model: posix
InstalledDir: /home/mmao/ti/ccs1110/ccs/tools/compiler/ti-cgt-armllvm_1.3.0.LTS/bin
"/home/mmao/ti/ccs1110/ccs/tools/compiler/ti-cgt-armllvm_1.3.0.LTS/bin/tiarmlnk" --search_path _build/TI_ARMLLVM/HSM/lib/ --search_path /home/mmao/ti/ccs1110/ccs/tools/compiler/ti-cgt-armllvm_1.3.0.LTS/lib --search_path _build/TI_ARMLLVM/HSM/bin --search_path _build/TI_ARMLLVM/HOST/bin -I/home/mmao/ti/ccs1110/ccs/tools/compiler/ti-cgt-armllvm_1.3.0.LTS/lib -o _build/TI_ARMLLVM/TI_ARMLLVM -llibHSM.lib -llibHOST_tests.lib -llibHOST.lib --start-group -llibc++.a -llibc++abi.a -llibc.a -llibsys.a -llibsysbm.a -llibclang_rt.builtins.a -llibclang_rt.profile.a --end-group --cg_opt_level=0
warning: cannot resolve archive
/home/mmao/ti/ccs1110/ccs/tools/compiler/ti-cgt-armllvm_1.3.0.LTS/lib/libc++
.a to a compatible library, as no input files have been encountered
warning: cannot resolve archive
/home/mmao/ti/ccs1110/ccs/tools/compiler/ti-cgt-armllvm_1.3.0.LTS/lib/libc++
abi.a to a compatible library, as no input files have been encountered
warning: cannot resolve archive
/home/mmao/ti/ccs1110/ccs/tools/compiler/ti-cgt-armllvm_1.3.0.LTS/lib/libc.a
to a compatible library, as no input files have been encountered
warning: cannot resolve archive
/home/mmao/ti/ccs1110/ccs/tools/compiler/ti-cgt-armllvm_1.3.0.LTS/lib/libsys
.a to a compatible library, as no input files have been encountered
warning: cannot resolve archive
/home/mmao/ti/ccs1110/ccs/tools/compiler/ti-cgt-armllvm_1.3.0.LTS/lib/libsys
bm.a to a compatible library, as no input files have been encountered
warning: cannot resolve archive
/home/mmao/ti/ccs1110/ccs/tools/compiler/ti-cgt-armllvm_1.3.0.LTS/lib/libcla
ng_rt.builtins.a to a compatible library, as no input files have been
encountered
warning: cannot resolve archive
/home/mmao/ti/ccs1110/ccs/tools/compiler/ti-cgt-armllvm_1.3.0.LTS/lib/libcla
ng_rt.profile.a to a compatible library, as no input files have been
encountered
fatal error: no input files
tiarmclang: error: tiarmlnk command failed with exit code 1 (use -v to see invocation)
The libraries (libHSM.lib, libHOST_tests.lib, libHOST.lib) for linking are packed with tiarmar from object files built with tiarmclang in the same time.
How should I resolve this issue?
Thanks,
Matthew