Part Number: CCSTUDIO
Other Parts Discussed in Thread: CC1352P, CC2640R2F, UNIFLASH
When trying to debug project_zero_CC1352P_4_LAUNCHXL_tirtos7_ticlang on a new CC1352P-4 LaunchPad
- CCS12 crashed at the end of the automatic firmware update of XDS110 to version 3.0.0.20
- After CCS restart, program loads but CCS12 crashes before displaying "loading symbols"
This is possibly a CCS version problem:
I do not have any issue with CCS11 Version:11.1.0.00011(TI Clang 1.3.0.LTS or TI Clang 2.1.0.LTS)
Other information
- Advanced debug settings of CCS are identical in both CCS versions
- Debugging is ok (CCS12) with a custom board (CC2640R2F, old sdk, not clang compiler) and a standalone XDS110
- No impact of antivirus (I tried with Bitdefender off)
- Loading the program with standalone Uniflash 6.1.0(project_zero_CC1352P_4_LAUNCHXL_tirtos7_ticlang.hex) works and I can connect to the board
- Reloading XDS110 firmware (3.0.0.20) using "xdsdfu -f firmware_3.0.0.20.bin -r" does not change anything
CONFIGURATION
- Windows 10, 21H2, build 19044.1865, Pack 120.2212.4180.0
- Bitdefender Internet Security
- CC1352P-4 LaunchPad with on-board XDS110 debug probe (CC1352P1-4 Development Kit), BOM Rev A, FW SDK4.1 2029
- Project Zero from simplelink_cc13xx_cc26xx_sdk_6_20_00_29
- CCS 12 Version: 12.0.0.00009
- TI Clang 2.1.0.LTS
Running eclipsec led to another error : Failed to load class "org.slf4j.impl.StaticLoggerBinder"