Other Parts Discussed in Thread: SYSCONFIG, AM3356, AM3359
Hi.
I am developing HSR/PRP custom board by referring to ICE3359.
It was confirmed that the AM335x had two PRU MACs and two EMACs of 335x itself.
However, using the SYSCONFIG tool, we have confirmed that using four MACs at the same time is unreasonable
Is this right?
Is it impossible to do at least 2 PRU MAC and 1 EMAC?
I have one more question
To proceed with the above process, I would like to refer to pinmux
C:\ti\pdk_am335x_1_0_17\packages\ti\starterware\tools\pinmux_config\am335x
I checked the internal 'icev2_config.pinmux' file.
However, it does not seem to be linked to the actual ICE3359.
No pins used in ICE3359 have been added.
Please check it.
Thank you.
Below is a picture of icev2_config.pinmux for reference.
The PRU pin is not set either, is this right?
Also, I am using AM3356.