This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C5515 FDK Question



Hello,

 

I have additional questions regarding hte C5515 TI supplied demo application code.

While working with XDS5510 JTAG and CCS 4.2.3 version, I am reading through the CCS UART register values and they are different from what I write into those registers.

While reading those values by CPU and looking on to the variable value I get the correct value.

Is that a known problem?

 

One more additional question is: I do know about the CSL but I prefer to configure UART by myself on C5515.

The following is code doing that:

 

{

// Ensure UART has been resetted

while (SYS_PRCNTRLR & 0x0080)

;


// Ensure clock enabled for UART

SYS_PCGCR1 &= (~0x4);


// put both uart tx and rx into reset

UART_PWREMU_MGMT &= ~(0x6000);


// UART 8 least sig bits of divisor

UART_DLH = 0x41;

// UART 8 most significant bits of divisor

UART_DLH = 0;


UART_FCR = 1;


UART_LCR = 0x0003;


UART_MCR = 0;


UART_PWREMU_MGMT = 0x6001;

}

 

Then I write into the THR values and expecting to receive them on UART other side.

I do not see anything coming out...

The question is: suppose I set the system by teh help of the function TA_hal_Init_high_clk to the value of 115200 baudrate. What is wrong with my code that causes UART not to tx data?

 

Regards