Part Number: DRA756
Render node /dev/dri/renderD128 fails
Steps to reproduce:
#start weston using desktop shell export WAYLAND_DISPLAY=/run/wayland0 # Does not work. By default it tries to use the offscreen render node # /dev/dri/renderD128. weston-simple-dmabuf-egl # Output: #Warning: zwp_linux_explicit_synchronization_v1 not supported, # will not use explicit synchronization # PVR:(Error): PVRDisplayBufferCreate: Failed to create display buffer (err=13) [0, ] # PVR:(Error): PVRDRIPlaneCreate: Failed to create share/scanout/cursor buffer [0, ] # PVR:(Error): PVRDRIBufferCreate: Failed to create plane [0, ] # CreateImageShared: Failed to create buffer # create_bo failed # Does work when overriding dri device. weston-simple-dmabuf-egl -d /dev/dri/card0
Using: meta-ti/recipes-graphics/libgles/ti-sgx-ddk-um_1.17.4948957.bb