According to UG(EMIF16) :The EMIF16 module is intended to provide a glue-less interface to a variety of asynchronous memory devices like ASRAM, NOR and NAND memory. A total of 256M bytes of any of these memories can be accessed at any given time via four chip selects with 64M byte access per chip select.
q:Does 6678 support a maximum addressing of 64M byte NAND FLASH over a chip select . if not , is there a limit of addressing when interfaceing a NAND FLASH with 6678 over one chip select?