Other Parts Discussed in Thread: OMAP-L138, OMAPL138
hi,
I have a problem.can not boot。I am using custom board and external memory is MT46H32M16 -LFBF-6B (mDDR ).I think UBL found boot,but can not booting at 0xC1080000.Im using
Serial Boot and Flash Loading Utility for OMAP-L138.I have m
odified the parameters passed to the function DEVICE_ExternalMemInit to match the mDDR timing requirements for the custom board(DEVICE.C,OMAP-L138/Common/src) Uboot is my application (.out file) and generated bin file using aisgen utility.and in my terminal output is comming like:
C:\Documents and Settings\user\My Documents\reshmi\sfh_31\OMAP-L138\GNU>sfh_OMAP-L138.exe -flashType SPI_MEM -flash G:\ubl_31\ubl_OMAPL138_SPI_MEM.bin G:\arm_boot\spi.bin -v
-----------------------------------------------------
TI Serial Flasher Host Program for OMAP-L138
(C) 2011, Texas Instruments, Inc.
Ver. 1.67
-----------------------------------------------------
Platform is Windows.
[TYPE] UBL and application image
[UBL] G:\ubl_31\ubl_OMAPL138_SPI_MEM.bin
[APP IMAGE] G:\arm_boot\spi.bin
[TARGET] OMAPL138
[DEVICE] SPI_MEM
Attempting to connect to device COM1...
Press any key to end this program at any time.
(AIS Parse): Read magic word 0x41504954.
(AIS Parse): Waiting for BOOTME... (power on or reset target now)
(AIS Parse): Read invalid BOOTME string.
(AIS Parse): Boot aborted.
Booting SFT failed. Trying again (you may need to reset the target)...
(AIS Parse): Read magic word 0x41504954.
(AIS Parse): Waiting for BOOTME... (power on or reset target now)
(AIS Parse): BOOTME received!
(AIS Parse): Performing Start-Word Sync...
(AIS Parse): Performing Ping Opcode Sync...
(AIS Parse): Processing command 0: 0x58535901.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Loading section...
(AIS Parse): Loaded 8704-Byte section to address 0x80000000.
(AIS Parse): Processing command 1: 0x58535901.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Loading section...
(AIS Parse): Loaded 824-Byte section to address 0x80002200.
(AIS Parse): Processing command 2: 0x58535906.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Performing jump and close...
(AIS Parse): AIS complete. Jump to address 0x80000000.
(AIS Parse): Waiting for DONE...
(AIS Parse): Boot completed successfully.
Waiting for SFT on the OMAP-L138...
Target: BOOTUBL
Target: DONE
Flashing UBL G:\ubl_31\ubl_OMAPL138_SPI_MEM.bin (8148 bytes) at 0x00000000
Target: INFO: SPI Memory Initialization passed.
Target: Flashing UBL...
Target: SENDIMG
Target: BEGIN
100% [ ████████████████████████████████████████████████████████████ ]
Image data transmitted over UART.
Target: DONE
0% [ ------------------------------------------------------------ ]
0% Programming UBL into flash...
100% ████████████████████████████████████████████████████████████
Verifying...
100% ████████████████████████████████████████████████████████████
UBL programming complete
Target: DONE
Flashing application G:\arm_boot\spi.bin (1672 bytes)
Target: SENDIMG
Target: BEGIN
100% [ ████████████████████████████████████████████████████████████ ]
Image data transmitted over UART.
Target: DONE
0% [ ------------------------------------------------------------ ]
Programming application into flash...
100% ████████████████████████████████████████████████████████████
Verifying... 0010000
100% ████████████████████████████████████████████████████████████
Application programming complete
Target: DONE
Target: DONE
Operation completed successfully.
And when i switch to Spi boot mode output is like:
OMAP-L138 initialization passed!
Booting TI User Boot Loader
UBL Version: 1.65
UBL Flashtype: SPI
Starting SPI memory Copy...
Valid magicnum, 0x55424CBB, found at offset 0x00010000.
DONE
Jumping to entry point at 0xC1080000.
Kindly suggest me fixing this issue?