My customer ran into an issue when testing RS-485 interfaces using SDK 8.02.00.24 (Kernel 5.10). This resulted in missing communication during system test. Same HW with earlier SDK 4.03.00.05 (Kernel 4.9) is working.
In addition they ported omap-serial.c from 4.9 to 5.10. This is also working. They are asking for 5.10 release with a working RS-485 driver. Any info what was recently changed in that drivers?
Regards, Frank