Hello,
I am working with AM3715 based design board on android 2.2 Devkit.
Could you please let me know what all changes are needed to support 512 MB DDR SDRAM for the same? My linux kernel version is 2.6.32.
Thanks,
-Ninad.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am working with AM3715 based design board on android 2.2 Devkit.
Could you please let me know what all changes are needed to support 512 MB DDR SDRAM for the same? My linux kernel version is 2.6.32.
Thanks,
-Ninad.
Have you looked at http://processors.wiki.ti.com/index.php/Setting_up_AM37x_SDRC_registers
Regards,
Vaibhav
Dear Vaibhav,
Thank you for the reply.
I am setting this registers for CS0 and CS1 and able to detect the 512 MB of size after reading SDRC_CS_CFG. x-loader loads the u-boot and s_init is also successful where we initialize the clocks, gpios and memory. In mem_init there is a early initialization for CS0 bank and I have added a code for initializing CS1 too here but even though start_armboot() function never gets called.
Could you please let me know what am I missing? any more changes are needed? any suggestions?
Thanks,
-Ninad.
Hi,
SDRAM init is handled by the x-loader only. You can refer to the function make_cs1_contiguous() under "board/omap3evm/omap3evm.c" in the x-loader sources for using two chip selects. This enables a stacked configuration of 256MB with each CS having 128MB and you could use this as a reference.
Note that U-Boot SDRAM code is never executed as U-Boot is already running for RAM. The SDRAM code in U-Boot is present there just for the sake of completion. So any SDRAM issues that you might face would need to be in x-loader.
Regards,
Vaibhav
Dear Vaibhav,
You are right, mem_init never gets called in u-boot because its already in RAM.
And yes I did chnage the make_cs1_contiguous() code for considering the configuration of 512MB with each CS having 256MB and now all the SDRC registers seems proper. But results are same as I posted earlier.
Thanks,
-Ninad.