This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM64X: How to Enable Cut-Through on ICSSG

Part Number: PROCESSOR-SDK-AM64X

Dear forum,

I have the AM64 EVM PROC101B. This board has two ethernet ports on the ICSS, and one on the CPSW. The instructions for enabling cut-through on the CPSW are pretty clear.

How can I enable cut-through between the ICSS ports? I believe the ICSS ports are eth1 and eth2, which are ports 1 and 2. So maybe the procedure is the same, i.e. write bits to the cut_thru_r/tx_pri_mask.

In our production system we intend to have four ethernet ports. Two on ICSSG0, and two on CPSW. Will we also be capable of enabling cut-through for both subsystems? I understand cut-through can't be enabled for traffic between ICSSG <-> CPSW.

Regards,
Brian