Part Number: AM625
We are using AM6254 in our design, We have few clarifications:
1, Do we need different external clock sources for main domain and MCU domain - If not, how are we achieving this MCU isolation from Main domain
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM625
We are using AM6254 in our design, We have few clarifications:
1, Do we need different external clock sources for main domain and MCU domain - If not, how are we achieving this MCU isolation from Main domain
1) AM62x provides a several optional clock inputs, WKUP_LFOSC0, AUDIO_EXT_REFCLK[1:0], EXT_REFCLK1, and MCU_EXT_REFCLK0. You should search the device TRM for each clock input to understand which internal modules can be clocked form each of these optional clock inputs. Then you need to determine if your specific system implementation is able to use one of the internal clock references or requires a external clock.
2) The internal 32k clock is generated from a integer divider of HFOSC operating frequency, which only supports 24 MHz , 25 MHz, or 26 MHz. For example, If HFOSC = 25 MHz, the internal 32k clock will be (25000000/95)/8= 32,894.7368 Hz or (25000000/96)/8= 32,552.0833 Hz. You may need to use WKUP_LFOSC0 if your application requires the internal 32k clock to be exactly 32,768 Hz.
3) Backup boot mode is only executed if primary boot mode fails. The boot mode/sequence selected depends on your specific system requirements. Please refer to the Initialization chapter in the device TRM for more details.
Regards,
Paul