Other Parts Discussed in Thread: OMAP5912, OMAP5910
Hi, I'm trying to compile a project that is set as huge memory model, but ccv4 informs me that 'Huge memory model not supported for CPU revisions 1 or 2'. Is it right that I cannot use that memory model for the C5515? When I put 'list' in the silicon version field in the build options i get the following list. Which of these is the bst choice, or have a configured something else incorrectly? cpu, cpu:0, cpu:1, cpu:1.0, cpu:1.1, cpu:1.X, cpu:2, cpu:2.0, cpu:2.1, cpu:2.2, cpu:2.X, cpu:3, cpu:3.0, cpu:3.1, cpu:3.2, cpu:3.21, cpu:3.3, cpu:3.X, cpu+, cpu+:1, , cpu+:2, plus, plus:1, plus:2, 5510, 5510:0, 5510:1, 5510:1.0, 5510:1.0A, 5510:1.1, 5510:1.1A, 5510:1.2, 5510:1.X, 5510:2, 5510:2.0, 5510:2.1, 5510:2.2, 5510:2.X, 5510A, 5501, 5501:1, 5501:1.0, 5502, 5502:1, 5502:1.0, 5503, 5503:1, 5503:1.0, 5504, 5504:1, 5504:1.0, 5505, 5505:1, 5505:1.0, 5506, 5506:1, 5506:1.0, 5507, 5507:1, 5507:1.0, 5509, 5509:A, 5509:B, 5509:C, 5509:D, 5509:E, 5509:F, 5509A, 5561, 5561:1, 5561:1.0, 5561:2, 5561:2.0, 5561:2.1, 5561:2.2, 561:2.X, DA250, DA250:1, DA250:1.0, DA250:1.1, DA250:1.X, DA250:2, DA250:2.0, DA250:2.05, DA250:2.1, DA250:2.X, DA250:3, DA250:3.0, DA250:3.1, DA250:3.2, DA250:3.X, DA255, DA255:1, DA255:1.0, DA255:1.1, DA255:1.X, OMAP1510, OMAP1610, OMAP1611, OMAP1612, OMAP1710, OMAP2140, OMAP2420, OMAP5903, OMAP5905, OMAP5907, OMAP5910, OMAP5912