Part Number: PROCESSOR-SDK-AM62X
Other Parts Discussed in Thread: SK-AM62
Hi everyone,
i am pretty new working with linux enviroment and i need hand to compile a simple test application on linux machine running Ubuntu 18.04.
I am successfully compiling a simple test program on sk-am62, i've created a file called ee_test.c :
// include file con le strutture per la periferica
#include <linux/i2c-dev.h>
// #include <linux/i2c-smbus.h>
#include <stdio.h>
//indirizzo della EEPROM a cui leggere
#define EE_ADDRESS 0x51
#define I2C_NUMBER 0
char dev_prefix[20] = "/dev/i2c-";
char dev_name[20];
int perif_num = 0;
int num;
int main(void) {
// completa il nome della periferica
num = snprintf(dev_name, sizeof(dev_name), "%s%d",dev_prefix,perif_num);
// test per vedere se ha scrittop giusto
printf("%s\n", dev_name);
return 0;
}
// eof
if i do that from sk-am62, everything works fine, the programs compile and run without problem.
Now i want to cross compile it on Ubuntu, because working with source files inside sk-am62 is hard, since i don t have a text editor inside arago linux and i don t know how to edit sorce files.
i created a makefile in my Ubuntu:
# ------------------------------------------------------------------------- # Makefile di compilazione per programma di test i2c su linux Arago # ------------------------------------------------------------------------- PLATFORM=am62x ARCH=arm64 PSDK_PATH=/home/ema/psdk/ TOOLS_PATH=$(PSDK_PATH)linux-devkit/sysroots/ BIN_PATH=$(TOOLS_PATH)x86_64-arago-linux/usr/bin/ CC_PREFIX=aarch64-none-linux-gnu- CC = $(BIN_PATH)$(CC_PREFIX)gcc CC_64 = $(BIN_PATH)$(CC_PREFIX)g++ AR_64 = $(BIN_PATH)$(CC_PREFIX)ar DBG_FLAGS=-g3 -gdwarf-2 -std=c++11 SRC=./ee_read.c OUT=ee_read INC_PATH=$(TOOLS_PATH)aarch64-linux/usr/include/ INC_LNX_PATH=$(PSDK_PATH)board-support/linux-rt-5.10.109+gitAUTOINC+d9ee8a25c2-gd9ee8a25c2/include/ INC_ASM=$(INC_LNX_PATH)asm-generic/ INC= -I . -I $(INC_PATH) -I $(INC_LNX_PATH) #normal debug: $(CC) $(DBG_FLAGS) $(SRC) $(INC) -o $(OUT) #pulisce compilazione clean: rm -f *.o $(OUT) lib*.a
but when i try to run it, it gives a lot of error in header files, please help to find out what i m doing wrong, here is output result:
/home/ema/psdk/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/aarch64-none-linux-gnu-gcc -g3 -gdwarf-2 ./ee_read.c -I . -I /home/ema/psdk/linux-devkit/sysroots/aarch64-linux/usr/include/ -I /home/ema/psdk/board-support/linux-rt-5.10.109+gitAUTOINC+d9ee8a25c2-gd9ee8a25c2/include/ -o ee_read
In file included from /home/ema/psdk/board-support/linux-rt-5.10.109+gitAUTOINC+d9ee8a25c2-gd9ee8a25c2/include/linux/kcsan-checks.h:7,
from /home/ema/psdk/board-support/linux-rt-5.10.109+gitAUTOINC+d9ee8a25c2-gd9ee8a25c2/include/asm/rwonce.h:27,
from /home/ema/psdk/board-support/linux-rt-5.10.109+gitAUTOINC+d9ee8a25c2-gd9ee8a25c2/include/linux/compiler.h:248,
from /home/ema/psdk/board-support/linux-rt-5.10.109+gitAUTOINC+d9ee8a25c2-gd9ee8a25c2/include/uapi/linux/i2c-dev.h:28,
from /home/ema/psdk/board-support/linux-rt-5.10.109+gitAUTOINC+d9ee8a25c2-gd9ee8a25c2/include/linux/i2c-dev.h:12,
from ./ee_read.c:13:
/home/ema/psdk/board-support/linux-rt-5.10.109+gitAUTOINC+d9ee8a25c2-gd9ee8a25c2/include/linux/compiler_attributes.h:64: warning: "__always_inline" redefined
64 | #define __always_inline inline __attribute__((__always_inline__))
|
In file included from /home/ema/psdk/board-support/linux-rt-5.10.109+gitAUTOINC+d9ee8a25c2-gd9ee8a25c2/include/linux/stddef.h:5,
from /home/ema/psdk/linux-devkit/sysroots/aarch64-linux/usr/include/linux/posix_types.h:5,
from /home/ema/psdk/board-support/linux-rt-5.10.109+gitAUTOINC+d9ee8a25c2-gd9ee8a25c2/include/uapi/linux/types.h:14,
from /home/ema/psdk/board-support/linux-rt-5.10.109+gitAUTOINC+d9ee8a25c2-gd9ee8a25c2/include/linux/types.h:6,
from /home/ema/psdk/board-support/linux-rt-5.10.109+gitAUTOINC+d9ee8a25c2-gd9ee8a25c2/include/uapi/linux/i2c-dev.h:27,
from /home/ema/psdk/board-support/linux-rt-5.10.109+gitAUTOINC+d9ee8a25c2-gd9ee8a25c2/include/linux/i2c-dev.h:12,
from ./ee_read.c:13:
/home/ema/psdk/board-support/linux-rt-5.10.109+gitAUTOINC+d9ee8a25c2-gd9ee8a25c2/include/uapi/linux/stddef.h:5: note: this is the location of the previous definition
5 | #define __always_inline inline
|
In file included from /home/ema/psdk/board-support/linux-rt-5.10.109+gitAUTOINC+d9ee8a25c2-gd9ee8a25c2/include/linux/compiler.h:248,
from /home/ema/psdk/board-support/linux-rt-5.10.109+gitAUTOINC+d9ee8a25c2-gd9ee8a25c2/include/uapi/linux/i2c-dev.h:28,
from /home/ema/psdk/board-support/linux-rt-5.10.109+gitAUTOINC+d9ee8a25c2-gd9ee8a25c2/include/linux/i2c-dev.h:12,
from ./ee_read.c:13:
/home/ema/psdk/board-support/linux-rt-5.10.109+gitAUTOINC+d9ee8a25c2-gd9ee8a25c2/include/asm/rwonce.h:64:31: error: expected ‘;’ before ‘unsigned’
64 | static __no_sanitize_or_inline
| ^
| ;
65 | unsigned long __read_once_word_nocheck(const void *addr)
| ~~~~~~~~
/home/ema/psdk/board-support/linux-rt-5.10.109+gitAUTOINC+d9ee8a25c2-gd9ee8a25c2/include/asm/rwonce.h:82:28: error: expected ‘;’ before ‘unsigned’
82 | static __no_kasan_or_inline
| ^
| ;
83 | unsigned long read_word_at_a_time(const void *addr)
| ~~~~~~~~
In file included from ./ee_read.c:15:
/home/ema/psdk/linux-devkit/sysroots/aarch64-linux/usr/include/stdio.h:77:19: error: conflicting types for ‘ssize_t’
77 | typedef __ssize_t ssize_t;
| ^~~~~~~
In file included from /home/ema/psdk/board-support/linux-rt-5.10.109+gitAUTOINC+d9ee8a25c2-gd9ee8a25c2/include/uapi/linux/i2c-dev.h:27,
from /home/ema/psdk/board-support/linux-rt-5.10.109+gitAUTOINC+d9ee8a25c2-gd9ee8a25c2/include/linux/i2c-dev.h:12,
from ./ee_read.c:13:
/home/ema/psdk/board-support/linux-rt-5.10.109+gitAUTOINC+d9ee8a25c2-gd9ee8a25c2/include/linux/types.h:60:26: note: previous declaration of ‘ssize_t’ was here
60 | typedef __kernel_ssize_t ssize_t;
| ^~~~~~~
Makefile:29: recipe for target 'debug' failed
make: *** [debug] Error 1i am using Ubuntu 18.04 as os, and i have processor sdk 08.03.00.19 installed,
what are the correct paths for include files, to successfully cross-compile?? are there any reference project for cross-compile for this board?
thank you
Emanuele Peruzzi