Using the C6748 SOM EVM from Logic PD, CCSv4
Attempting to launch target, the following error message appears.
Error connecting to the target:
(Error -180 @ 0x0)
The controller has detected a target power loss.
The user must turn-on or connect the power supply for the target.
(Release 5.0.333.0)
Steps taken so far:
Verified that power is attached and turned on.
Tried another "known good" power supply.
How do i diagnose this furtther? What is the solution?