Other Parts Discussed in Thread: PMP
I rebuilt the linux kernel to include firewire support for a 1394 compatible USB camera, followed by rebuilding and installing the modules including syslink. The EVM still boots, but I'm getting errors in the boot log. In particular, it is complaining that it cannot find syslink.ko, yet it is there, in targetfs/lib/modules/2.6.37/kernel/drivers/dsp/. The relevent errors are bolded.
U-Boot 2010.06 (May 12 2011 - 15:37:57)
TI8168-GP rev 1.0
ARM clk: 987MHz
DDR clk: 398MHz
I2C: ready
DRAM: 2 GiB
NAND: HW ECC Hamming Code selected
256 MiB
:,;;:;:;;;;;;;;r;;:,;;:;:;;;;;;;;:,;;:;:;;;;;;;;:,;;:;:;;;;;;;;:;;;;;;;;:,;;:;:
;,;:::;;;;r;;;rssiSiS552X5252525259GX2X9hX9X9XX2325S55252i5:,;;:;:;;;;;;;;:,;;:
;:;;;;;;;rrssSsS52S22h52299GGAAMHMM#BBH#B#HMM#HMBA&&XX2255S2S5Si:,;;:;:;;;;;;;;
;:;;r;;rsrrriiXS5S329&A&MH#BMB#A&9XXA252GXiSXX39AAMMMBB&G22S5i2SSiiiisi:,;;:;:;
;;;;;r;rr2iisiih393HB#B#AA99i22irrrX3X52AGsisss2Xii2299HBMA&X2S5S5iSiisSsi:,;;:
r:r;rrsrsihXSi2&##MHB&Ahh3AGHGA9G9h&#H##@@@##MAMMXXX9SSS29&&HGGX2i5iisiiisisi:,
;;rrrrsSiiiA&ABH&A9GAGhAhBAMHA9HM@@@@@@@@@@@@@@@@@@@HHhAh2S2SX9&Gh22SSiisiiisii
r:rrssisiS2XM##&h3AGAX&3GG3Ssr5H@M#HM2; ;2X&&&MHMB###GBB#B&XXSSs529XX55iSsisisi
r;rsrisSi2XHAhX99A3XXG&&XS;:,rH#HGhAS @@@@3rs2XBM@@A552&&AHA2XiisSS252SSsisSs
r;issi5S22&&3iSSX292&hXsr;;:;h@&G339&S9@@@@2@MA&9&HB##Xris29ABMAAX2ir;rsSi5iss5
rrsSi2XhG&9GXh399&X99i;;;;;;r#H&293H9X#@@@@@@@B&9GhAH@XrrsrsiXABHB&HG2rr;rrSiSi
;:rsisS599&AA9XG&3A35r;:::;,;BMh&&2iX5A@@@@@@@&392X5GB2;;;r;iSX393A##A&Xi:::rsi
;:rss552222X553&XHMhir;;::,:,h#HhGSXhG3#@@@@#AXXS2XAHA;::;;;;ss55XShBA3239r:,;;
r;ii2S5SSi2i53hirsh2srr::,,,,;MMXX359&Ah3h&Si59SX99A#i:,::::;;sri2,.2r;:SGAr;,:
;:;rrrrssiriXGSi::shs;;;,,,:,,rBBA9h5s5h5iS5isi2SAHB5:,,,:::;rrs5&SrisSX5Srrr:,
;,r;;;;rsriSSrrrr;;5Xrr;;,:,,.,;9AA2SsisS5323XXXG9&i:.,,::;;r;;;srrrrrr;;:;::::
:,;r;r;rrissrrr;:;::;s;;;;,:,,..,r293h222hXXAAGGGX;:,,,:,:,::;:;::,:,,,,...,,,,
;,;;;;rrrrrrrrirr;,.,,:::::::,,,,.,;SX&ABAB2hhXir:,,.,,.,,:,,,,..,,,..,..,,,..:
:.:;:;;;:;;;;r;rrs;:.. ,,:::::,:,:,,.::rrsrr;;,,.......,..,....,,,,,,,...,.,,:,
:.:::,::::::;;r;rrr;:.......,.,.,,:::,,...............,,::.,,,,:,::,,:,:,,,:,;:
,.::,:,,,,,;;;;;;;;r;;::,..............................;;;:;::::,:::::::,:,:,,,
: ,,:,,,,,,,,,,,,,:;rrr;;:;,,,,,,,::,.,.:.,.,;s,:;;;;:;:;;;;;::::,:::,:::,:,:,:
,.,,,,,,,...,,.,,....................................:,............:,,,:,:,,,,,
Net: Detected MACID:64:7b:d4:10:f0:5a
Ethernet PHY: GENERIC @ 0x01
DaVinci EMAC
Hit any key to stop autoboot: 3 2 1 0
Using DaVinci EMAC device
TFTP from server 192.168.1.100; our IP address is 192.168.1.10
Filename 'uImage-dm816x-evm.bin'.
Load address: 0x81000000
Loading: *#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
###########
done
Bytes transferred = 2383028 (245cb4 hex)
## Booting kernel from Legacy Image at 81000000 ...
Image Name: Linux-2.6.37
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2382964 Bytes = 2.3 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Linux version 2.6.37 (lholeva@UbuntuHost) (gcc version 4.3.3 (Sourcery G++ Lite
2009q1-203) ) #2 Mon May 23 12:15:36 EDT 2011
CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: ti8168evm
bootconsole [earlycon0] enabled
vram size = 52428800 at 0
reserved size = 52428800 at 0
FB: Reserving 52428800 bytes SDRAM for VRAM
Memory policy: ECC disabled, Data cache writeback
OMAP chip is TI8168 1.0
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 52224
Kernel command line: console=ttyO2,115200n8 rootwait rw mem=256M earlyprintk vra
m=50M ti816xfb.vram=0:16M,1:16M,2:6M root=/dev/nfs nfsroot=192.168.1.100:/home/l
holeva/targetfs ip=192.168.1.10:192.168.1.100:192.168.1.100:255.255.255.0:Ubuntu
host:eth0:off
PID hash table entries: 1024 (order: 0, 4096 bytes)
Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
Memory: 206MB = 206MB total
Memory: 203560k/203560k available, 58584k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
vmalloc : 0xd0800000 - 0xf8000000 ( 632 MB)
lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
modules : 0xbf000000 - 0xc0000000 ( 16 MB)
.init : 0xc0008000 - 0xc0035000 ( 180 kB)
.text : 0xc0035000 - 0xc0482000 (4404 kB)
.data : 0xc0482000 - 0xc04c3460 ( 262 kB)
SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
NR_IRQS:407
IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
Total of 128 interrupts on 1 active controller
GPMC revision 6.0
Trying to install interrupt handler for IRQ400
Trying to install interrupt handler for IRQ401
Trying to install interrupt handler for IRQ402
Trying to install interrupt handler for IRQ403
Trying to install interrupt handler for IRQ404
Trying to install interrupt handler for IRQ405
Trying to install interrupt handler for IRQ406
Trying to install type control for IRQ407
Trying to set irq flags for IRQ407
OMAP clockevent source: GPTIMER1 at 27000000 Hz
Console: colour dummy device 80x30
Calibrating delay loop... 986.31 BogoMIPS (lpj=4931584)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
devtmpfs: initialized
omap_voltage_early_init: voltage driver support not added
regulator: core version 0.5
regulator: dummy:
NET: Registered protocol family 16
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
omap_mux_init: Add partition: #1: core, flags: 0
_omap_mux_get_by_name: Could not find signal i2c2_scl.i2c2_scl
_omap_mux_get_by_name: Could not find signal i2c2_sda.i2c2_sda
NOR: Can't request GPMC CS
registered ti816x_vpss device
pm_dbg_init: only OMAP3 supported
Registered ti81xx_fb device
ti816x_pcie: Invoking PCI BIOS...
ti816x_pcie: Setting up Host Controller...
ti816x_pcie: Register base mapped @0xd0820000
ti816x_pcie: Starting PCI scan...
PCI: bus0: Fast back to back transfers enabled
bio: create slab <bio-0> at 0
vgaarb: loaded
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz
omap_i2c omap_i2c.2: bus 2 rev4.0 at 100 kHz
Advanced Linux Sound Architecture Driver Version 1.0.23.
Switching to clocksource gp timer
musb-hdrc: version 6.0, host, debug=0
musb-hdrc musb-hdrc.0: dma type: dma-cppi41
registerd cppi-dma Intr @ IRQ 17
Cppi41 Init Done
musb-hdrc: kernel must blacklist external hubs
musb-hdrc musb-hdrc.0: MUSB HDRC host driver
musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: MUSB HDRC host driver
usb usb1: Manufacturer: Linux 2.6.37 musb-hcd
usb usb1: SerialNumber: musb-hdrc.0
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
musb-hdrc musb-hdrc.0: USB Host mode controller at d080c000 using DMA, IRQ 18
musb-hdrc musb-hdrc.1: dma type: dma-cppi41
musb-hdrc: kernel must blacklist external hubs
musb-hdrc musb-hdrc.1: MUSB HDRC host driver
musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2
usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb2: Product: MUSB HDRC host driver
usb usb2: Manufacturer: Linux 2.6.37 musb-hcd
usb usb2: SerialNumber: musb-hdrc.1
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
musb-hdrc musb-hdrc.1: USB Host mode controller at d081e800 using DMA, IRQ 19
NET: Registered protocol family 2
IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
TCP established hash table entries: 8192 (order: 4, 65536 bytes)
TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
NetWinder Floating Point Emulator V0.97 (double precision)
sr1_fck HVT rate = 125000000
sr2_fck SVT rate = 125000000
SmartReflex Driver: Un-Characterized silicon found
SmartReflex Driver is notinitialized
omap-iommu omap-iommu.0: ducati registered
omap-iommu omap-iommu.1: sys registered
JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
msgmni has been set to 397
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0
omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
console [ttyO2] enabled, bootconsole disabled
console [ttyO2] enabled, bootconsole disabled
brd: module loaded
loop: module loaded
ahci ahci.0: forcing PORTS_IMPL to 0x3
ahci ahci.0: AHCI 0001.0100 32 slots 2 ports 3 Gbps 0x3 impl platform mode
ahci ahci.0: flags: ncq sntf pm led clo only pmp pio slum part ccc
scsi0 : ahci_platform
scsi1 : ahci_platform
ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x100 irq 16
ata2: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x180 irq 16
m25p80 spi1.0: w25x32 (4096 Kbytes)
Creating 4 MTD partitions on "spi_flash":
0x000000000000-0x000000040000 : "U-Boot"
0x000000040000-0x000000042000 : "U-Boot Env"
0x000000042000-0x0000002c2000 : "Kernel"
0x0000002c2000-0x000000400000 : "File System"
omap2-nand driver initializing
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xca (Micron )
Creating 5 MTD partitions on "omap2-nand.0":
0x000000000000-0x000000260000 : "U-Boot"
0x000000260000-0x000000280000 : "U-Boot Env"
0x000000280000-0x0000006c0000 : "Kernel"
0x0000006c0000-0x00000cee0000 : "File System"
0x00000cee0000-0x000010000000 : "Reserved"
davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
davinci_mdio davinci_mdio.0: detected phy mask fffffffd
davinci_mdio.0: probed
davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver dm9601
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
mice: PS/2 mouse device common for all mice
i2c /dev entries driver
Linux video capture interface: v2.00
usbcore: registered new interface driver uvcvideo
USB Video Class driver (v1.0.0)
OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec
PSTATE 1f20000
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
usbcore: registered new interface driver snd-usb-audio
1-0018 supply IOVDD not found, using dummy regulator
1-0018 supply DVDD not found, using dummy regulator
1-0018 supply AVDD not found, using dummy regulator
1-0018 supply DRVDD not found, using dummy regulator
asoc: tlv320aic3x-hifi <-> davinci-mcasp.2 mapping ok
ALSA device list:
#0: TI81XX EVM
TCP cubic registered
NET: Registered protocol family 17
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
omap_voltage_late_init: Voltage driver support not added
ata2: SATA link down (SStatus 0 SControl 300)
ata1: SATA link down (SStatus 0 SControl 300)
usb 2-1: new low speed USB device using musb-hdrc and address 2
usb 2-1: New USB device found, idVendor=046d, idProduct=c016
usb 2-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
usb 2-1: Product: Optical USB Mouse
usb 2-1: Manufacturer: Logitech
input: Logitech Optical USB Mouse as /devices/platform/musb-ti81xx/musb-hdrc.1/u
sb2/2-1/2-1:1.0/input/input0
generic-usb 0003:046D:C016.0001: input: USB HID v1.10 Mouse [Logitech Optical US
B Mouse] on usb-musb-hdrc.1-1/input0
davinci_mdio davinci_mdio.0: resetting idled controller
net eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, id=282f014)
IP-Config: Complete:
device=eth0, addr=192.168.1.10, mask=255.255.255.0, gw=192.168.1.100,
host=Ubuntuhost, domain=, nis-domain=(none),
bootserver=192.168.1.100, rootserver=192.168.1.100, rootpath=
PHY: 0:01 - Link is Up - 100/Full
VFS: Mounted root (nfs filesystem) on device 0:14.
devtmpfs: mounted
Freeing init memory: 180K
INIT: version 2.86 booting
Error opening /dev/fb0: No such file or directory
Please wait: booting...
Starting udev
udevd (75): /proc/75/oom_adj is deprecated, please use /proc/75/oom_score_adj in
stead.
udev: starting version 141
Root filesystem already rw, not remounting
Caching udev devnodes
Populating dev cachemv: cannot rename '/tmp/devices': No such file or directory
NET: Registered protocol family 10
ALSA: Restoring mixer settings...
NOT configuring network interfaces: / is an NFS mount
hwclock: can't open '/dev/misc/rtc': No such file or directory
No state is present for card EVM
Fri May 6 04:43:00 UTC 2011
Found hardware: "" "" "" "" ""
Hardware is initialized using a generic method
hwclock: can't open '/dev/misc/rtc': No such file or directory
No state is present for card EVM
INIT: Entering runlevel: 5
Starting system message bus: dbus.
Starting telnet daemon.
Loading HDVPSS Firmware
FATAL: Module syslink not found.
OsalDrv driver open: /dev/syslinkipc_Osal: No such file or directory
OsalDrv driver close: /dev/syslinkipc_Osal: Bad file descriptor
/dev/syslinkipc_MultiProc: No such file or directory
MultiProc driver close: : Bad file descriptor
SharedRegion driver open: : No such file or directory
SharedRegion driver close: : Bad file descriptor
/dev/syslinkipc_GateMP: No such file or directory
/dev/syslinkipc_MessageQ: No such file or directory
MessageQ driver close: : Bad file descriptor
Notify driver open: /dev/syslinkipc_Notify: No such file or directory
Notify driver close: /dev/syslinkipc_Notify: Bad file descriptor
ProcMgr driver open: /dev/syslinkipc_ProcMgr: No such file or directory
ProcMgr driver close: /dev/syslinkipc_ProcMgr: Bad file descriptor
/dev/syslinkipc_HeapBufMP: No such file or directory
/dev/syslinkipc_HeapMemMP: No such file or directory
/dev/syslinkipc_ListMP: No such file or directory
/dev/syslinkipc_RingIO: No such file or directory
RingIO driver close: : Bad file descriptor
/dev/syslinkipc_RingIOShm: No such file or directory
RingIO driver close: : Bad file descriptor
/dev/syslinkipc_ClientNotifyMgr: No such file or directory
ClientNotifyMgr driver close: : Bad file descriptor
/dev/syslinkipc_FrameQBufMgr: No such file or directory
FrameQBufMgr driver close: : Bad file descriptor
/dev/syslinkipc_FrameQ: No such file or directory
FrameQ driver close: : Bad file descriptor
/dev/syslinkipc_Ipc: No such file or directory
ProcMgr driver open: /dev/syslinkipc_ProcMgr: No such file or directory
ProcMgr driver close: /dev/syslinkipc_ProcMgr: Bad file descriptor
FIRMWARE: Could not open ProcMgr: -8
Simple mixer control 'Left PGA Mixer Mic3L',0
Capabilities: pswitch pswitch-joined penum
Playback channels: Mono
Mono: Playback [on]
Simple mixer control 'Left PGA Mixer Mic3R',0
Capabilities: pswitch pswitch-joined penum
Playback channels: Mono
Mono: Playback [on]
Simple mixer control 'Right PGA Mixer Mic3L',0
Capabilities: pswitch pswitch-joined penum
Playback channels: Mono
Mono: Playback [on]
Simple mixer control 'Right PGA Mixer Mic3R',0
Capabilities: pswitch pswitch-joined penum
Playback channels: Mono
Mono: Playback [on]
numid=1,iface=MIXER,name='PCM Playback Volume'
; type=INTEGER,access=rw---R--,values=2,min=0,max=127,step=0
: values=96,96
| dBscale-min=-63.50dB,step=0.50dB,mute=0
numid=37,iface=MIXER,name='PGA Capture Volume'
; type=INTEGER,access=rw---R--,values=2,min=0,max=119,step=0
: values=90,90
| dBscale-min=0.00dB,step=0.50dB,mute=0
vpss: Unknown symbol MultiProc_getId (err 0)
vpss: Unknown symbol Notify_sendEvent (err 0)
vpss: Unknown symbol Notify_registerEvent (err 0)
vpss: Unknown symbol Notify_unregisterEvent (err 0)
FATAL: Error inserting vpss (/lib/modules/2.6.37/kernel/drivers/video/ti81xx/vps
s/vpss.ko): Unknown symbol in movpss: Unknown symbol MultiProc_getId (err 0)
dule, or unknownvpss: Unknown symbol Notify_sendEvent (err 0)
parameter (see vpss: Unknown symbol Notify_registerEvent (err 0)
dmesg)
vpss: Unknown symbol Notify_unregisterEvent (err 0)
FATAL: Error inserting ti81xxfb (/lib/modules/2.6.37/kernel/drivers/video/ti81xx
/ti81xxfb/ti81xxfb.ko): Unknown symbol in module, or unknown parameter (see dmes
g)
open /dev/fb0: No such file or directory
cat: write error: No space left on device
cat: write error: No space left on device
FATAL: Module TI81xx_hdmi not found.
Starting syslogd/klogd: done
Starting thttpd.
ioctl FBIOGET_VSCREENINFO: Inappropriate ioctl for device
ioctl FBIOGET_VSCREENINFO: Inappropriate ioctl for device
expr: syntax error
Linux Frame Buffer Device Configuration Version 2.1 (23/06/1999)
(C) Copyright 1995-1999 by Geert Uytterhoeven
Usage: fbset [options] [mode]
Valid options:
General options:
-h, --help : display this usage information
--test : don't change, just test whether the mode is valid
-s, --show : display video mode settings
-i, --info : display all frame buffer information
-v, --verbose : verbose mode
-V, --version : print version information
-x, --xfree86 : XFree86 compatibility mode
-a, --all : change all virtual consoles on this device
Frame buffer special device nodes:
-fb <device> : processed frame buffer device
(default is /dev/fb0)
Video mode database:
-db <file> : video mode database file
(default is /etc/fb.modes)
Display geometry:
-xres <value> : horizontal resolution (in pixels)
-yres <value> : vertical resolution (in pixels)
-vxres <value> : virtual horizontal resolution (in pixels)
-vyres <value> : virtual vertical resolution (in pixels)
-depth <value> : display depth (in bits per pixel)
-nonstd <value> : select nonstandard video mode
-g, --geometry ... : set all geometry parameters at once
-match : set virtual vertical resolution by virtual resolution
Display timings:
-pixclock <value> : pixel clock (in picoseconds)
-left <value> : left margin (in pixels)
-right <value> : right margin (in pixels)
-upper <value> : upper margin (in pixel lines)
-lower <value> : lower margin (in pixel lines)
-hslen <value> : horizontal sync length (in pixels)
-vslen <value> : vertical sync length (in pixel lines)
-t, --timings ... : set all timing parameters at once
Display flags:
-accel <value> : hardware text acceleration enable (false or true)
-hsync <value> : horizontal sync polarity (low or high)
-vsync <value> : vertical sync polarity (low or high)
-csync <value> : composite sync polarity (low or high)
-gsync <value> : synch on green (false or true)
-extsync <value> : external sync enable (false or true)
-bcast <value> : broadcast enable (false or true)
-laced <value> : interlace enable (false or true)
-double <value> : doublescan enable (false or true)
-rgba <r,g,b,a> : recommended length of color entries
-grayscale <value> : grayscale enable (false or true)
Display positioning:
-move <direction> : move the visible part (left, right, up or down)
-step <value> : step increment (in pixels or pixel lines)
(default is 8 horizontal, 2 vertical)
Starting PVR
FATAL: Module omaplfb not found.
FATAL: Module bufferclass_ti not found.
/dev/mem opened.
Memory mapped at address 0x40231000.
Read at address 0x48180F04 (0x40231f04): 0x00000001
Write at address 0x48180F04 (0x40231f04): 0x00000000, readback 0x00000000
/dev/mem opened.
Memory mapped at address 0x400d9000.
Read at address 0x48180900 (0x400d9900): 0x00000102
Write at address 0x48180900 (0x400d9900): 0x00000002, readback 0x00000002
/dev/mem opened.
Memory mapped at address 0x4010e000.
Read at address 0x48180920 (0x4010e920): 0x00040002
Write at address 0x48180920 (0x4010e920): 0x00000002, readback 0x00000002
Calibrating touchscreen (first time only)ts_open: No such file or directory
.
Starting Matrix GUI application.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org dm816x-evm ttyO2
Arago 2011.02 dm816x-evm ttyO2
dm816x-evm login: root
root@dm816x-evm:~#
I notice that char/ti81xx_hdmi/TI81xx_hdmi.ko did not get remade. Perhaps I'm missing a selection in the menuconfig. Also, where in the target is the ordering of driver installation configured? I did not see something like rc.local in /etc/init.d/.
Update:
I found TI81XX_HDMI in menuconfig. It under character devices and was unchecked. I need to fix that. I also am having some issues with make linux as it appears to wipe-out my menuconfig selections, returning to the default.
Update Secundum:
I got TI81XX_hdmi to install, but I'm still missing a bunch of drivers under gpu/pvr/:
bufferclass_ti.ko omaplfb.ko pvrsrvkm.ko
where are the menuconfig selections for these?
Lee Holeva