This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Tirtos and Freertos

Part Number: TDA4VM
Other Parts Discussed in Thread: SYSBIOS

Hi team,

Here's an issue from the customer may need your help:

When upgrading RTOS SDK (SDK7.1 to SDK8.2), it has the following problem:

When using SDK7.1, the DMTimer was configured at sysbios_r5f.cfg as follows:

As configured above, a timer interrupt of 1 ms can be obtained through the timer_create, whereas after upgrading to SDK8.2 FreeRTOS, the previous sysbios_r5f.cfg no longer takes effect, resulting in an otherwise accurate 1-ms timer being out of order.

Could you help check this case? Thanks.

Best Regards,

Cherry