Part Number: AM625
Hello TI expert
We are working on the AM62xx series processor, and we like to know that what is the capability of the display devices & interface.
As per the datasheet first page each display support 1920x1080 @ 60fps,
If I consider AM62x starter kit (SK) evaluation module (EVM), Then I understand the 1st display would connect on 2 x 4 lanes LVDS, and the second display would connect on HDMI after 24-bit RGB parallel interface to HDMI conversion with help of SiI9022ACNU. please correct me if I am wrong. and please confirm resolution and frame rate mentioned above is correct for both displays or not?
Can you please let us know the 1st display manufacturer part no which is connected on LVDS and validated with AM62x starter kit (SK)? and share available information of 1st display with us? And please let us know at what max resolution and frame rate the same Display is validated?
if 2nd display is run on HDMI then the resolution & frame rate of 1st display (LVDS) will reduce or it will remain 1080p 60FPS?
-
Thanks,
Vaibhav kundariya