Hello,
I am new to TI processors, I am a Hardware person, i need some basic information about TI processors.
--> After Power ON, what is the status of the multiplexed pin,whether it is GPIO or it support corresponding alternative pin function?
-->At Device power OFF& power ON, what is STATE of each pin... Low, high or high impedance etc?
--> Where i could able to check the pin driving capacity and capacitance details of each pin?
-->What is the delay between given input clock and the derived output clocks? Is there any phase shift will be there?
-->What are all the key parameters i need to check while design with TI processors?
--> Is there any Hardware design guidelines document availble?
Thanks & Regards,
Thamizh