This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: SerDes interface level

Part Number: TDA4VM

Hi team,

Here're 2 questions from the customer may need your help:

1) When the SerDes interface of TDA4 is used as SGMII communication, is the differential logic level of the communication CML or LVDS? Or are both able to being supported through s/w configuration?

2) In the case of LVDS, is there a 100 ohm termination match and internal bias inside the chip? 

Thanks.

Best Regards,

Cherry