Part Number: TDA4VM
Hi team,
Here's an issue from the customer may need your help:
Development package: PROCESSOR-SDK-J721E
After qtcreator and source /Linux-devkit/environment-setup are installed on the PC, qmake builds the project .pro, which is an x86-based application.
Set the QMAKESPEC path to TI-processor-SDK-Linux-J7-EVM-08_02_00_03/targetNFS/usr/lib/mkspecs/Linux-g++, compiling the .pro file with qmake reported an error as follows:" Error: Could not find feature thread."
Referenced following 2 links to configure environment variables since it‘s not documented in PROCESSOR-SDK-J721E:
Could you help check this case? Thanks.
Best Regards,
Cherry