This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: ADC sample circuit design

Part Number: TDA4VM

Hi team,

Here're 2 questions from the customer may need your help:

1) Could you help check the following ADC sampling circuit design with the monitored power supply divided by resistors and connected to the ADC pin? Is it ok?

2) Regarding the ADC Input Impedance:

a. Is the ADC input impedance= 252.6ohm when SMPL_CLK = 60MHz?

b. ADC input impedance is 252.6ohm, is it required to add a voltage follower between the voltage divider circuit of the power supply to be monitored and the ADC pin for isolation?

Thanks.

Best Regards,

Cherry