This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP4 Blaze Video Capture

I have blaze development platform. It is running Ubuntu (Maverick).  I installed all  packages from TI PPA.

I am trying to capture video from cameras, using gstreamer but am having no luck.

 I only see /dev/video1, /dev/video2, and /dev/video3.

One of the simplest pipeline I tried was  gst-launch omx_camera ! v4l2sink which produced follwing errors :

system/domx/omx_rpc/src/omx_rpc.c:730   _RPC_ClientCreate()     ERROR: failed check: status >= 0
system/domx/omx_rpc/src/omx_rpc.c:730   _RPC_ClientCreate()     ERROR:  - returning error: RPC_OMX_RCM_ClientFail
system/domx/omx_rpc/src/omx_rpc.c:730   _RPC_ClientCreate()     ERROR: Error code: 0x70009
system/domx/omx_rpc/src/omx_rpc.c:730   _RPC_ClientCreate()     ERROR:  - RCM ClientCreate failed. Cannot Establish the connection
system/domx/omx_rpc/src/omx_rpc.c:192   RPC_InstanceInit()      ERROR: failed check: eRPCError == RPC_OMX_ErrorNone
system/domx/omx_rpc/src/omx_rpc.c:192   RPC_InstanceInit()      ERROR:  - returning error: eRPCError
system/domx/omx_rpc/src/omx_rpc.c:192   RPC_InstanceInit()      ERROR: Error code: 0x70009
system/domx/omx_rpc/src/omx_rpc.c:192   RPC_InstanceInit()      ERROR:  - Client create failed
system/domx/omx_proxy_common/src/omx_proxy_common.c:1841        OMX_ProxyCommonInit()   ERROR: failed check: eRPCError == RPC_OMX_ErrorNone
system/domx/omx_proxy_common/src/omx_proxy_common.c:1841        OMX_ProxyCommonInit()   ERROR:  - returning error: OMX_ErrorUndefined
system/domx/omx_proxy_common/src/omx_proxy_common.c:1841        OMX_ProxyCommonInit()   ERROR: Error code: 0x80001001
system/domx/omx_proxy_common/src/omx_proxy_common.c:1841        OMX_ProxyCommonInit()   ERROR:  - Error initializing RPC
video/omx_proxy_component/src/omx_proxy_camera.c:173    OMX_ComponentInit()     ERROR: ror in Initializing Proxy
Caught SIGSEGV accessing address (nil)
#0  0x2abd2fc6 in ?? ()
#1  0x2abd1c7e in ?? ()
Spinning.  Please run 'gdb gst-launch 13312' to continue debugging, Ctrl-C to quit, or Ctrl-\ to dump core.
^CCaught interrupt --

 

then I tried

gst-launch    v4l2src always-copy=false  --gst-debug-level=2 !  video/x-raw-yuv,width=160,height=120,framerate=30000/1001 ! fakesink -v produces following errors

Setting pipeline to PAUSED ...
0:00:00.151733398 13323   0x1f2050 WARN                    v4l2 v4l2_calls.c:491:gst_v4l2_open:<v4l2src0> error: Cannot identify device '/dev/video0'.
0:00:00.151855468 13323   0x1f2050 WARN                    v4l2 v4l2_calls.c:491:gst_v4l2_open:<v4l2src0> error: system error: No such file or directory
ERROR: Pipeline doesn't want to pause.
ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Cannot identify device '/dev/video0'.
Additional debug info:
v4l2_calls.c(491): gst_v4l2_open (): /GstPipeline:pipeline0/GstV4l2Src:v4l2src0:
system error: No such file or directory
Setting pipeline to NULL ...
Freeing pipeline ...

 

 v4l-info /dev/video3 display following :

### v4l2 device info [/dev/video3] ###
general info
    VIDIOC_QUERYCAP
        driver                  : "omap_wb"
        card                    : "omap_wb"
        bus_info                : ""
        version                 : 0.0.0
        capabilities            : 0x4000001 [VIDEO_CAPTURE,STREAMING]

standards

inputs

video capture
    VIDIOC_G_FMT(VIDEO_CAPTURE)
        type                    : VIDEO_CAPTURE
        fmt.pix.width           : 160
        fmt.pix.height          : 120
        fmt.pix.pixelformat     : 0x34424752 [RGB4]
        fmt.pix.field           : ANY
        fmt.pix.bytesperline    : 320
        fmt.pix.sizeimage       : 38400
        fmt.pix.colorspace      : JPEG
        fmt.pix.priv            : 0

controls

### video4linux device info [/dev/video3] ###
general info
    VIDIOCGCAP
        name                    : "omap_wb"
        type                    : 0x1 [CAPTURE]
        channels                : 0
        audios                  : 0
        maxwidth                : 0
        maxheight               : 0
        minwidth                : 48
        minheight               : 32

channels

tuner
ioctl VIDIOCGTUNER: Invalid argument

audio
ioctl VIDIOCGAUDIO: Invalid argument

picture
    VIDIOCGPICT
        brightness              : 0
        hue                     : 0
        colour                  : 0
        contrast                : 0
        whiteness               : 0
        depth                   : 16
        palette                 : unknown

buffer
ioctl VIDIOCGFBUF: Invalid argument

window
    VIDIOCGWIN
        x                       : 0
        y                       : 0
        width                   : 0
        height                  : 0
        chromakey               : 0
        flags                   : 0

/dev/video1 and /dev/video2 seems like output video devices.

 

Has anyone able to capture video on Blaze platform with Ubuntu?


I have tried several different piplines, but not having any luck.

 

If I use omx_camera as vedio source, it always fives following errors :

system/domx/omx_rpc/src/omx_rpc.c:730   _RPC_ClientCreate()     ERROR: failed check: status >= 0
system/domx/omx_rpc/src/omx_rpc.c:730   _RPC_ClientCreate()     ERROR:  - returning error: RPC_OMX_RCM_ClientFail
system/domx/omx_rpc/src/omx_rpc.c:730   _RPC_ClientCreate()     ERROR: Error code: 0x70009
system/domx/omx_rpc/src/omx_rpc.c:730   _RPC_ClientCreate()     ERROR:  - RCM ClientCreate failed. Cannot Establish the connection
system/domx/omx_rpc/src/omx_rpc.c:192   RPC_InstanceInit()      ERROR: failed check: eRPCError == RPC_OMX_ErrorNone
system/domx/omx_rpc/src/omx_rpc.c:192   RPC_InstanceInit()      ERROR:  - returning error: eRPCError
system/domx/omx_rpc/src/omx_rpc.c:192   RPC_InstanceInit()      ERROR: Error code: 0x70009
system/domx/omx_rpc/src/omx_rpc.c:192   RPC_InstanceInit()      ERROR:  - Client create failed
system/domx/omx_proxy_common/src/omx_proxy_common.c:1841        OMX_ProxyCommonInit()   ERROR: failed check: eRPCError == RPC_OMX_ErrorNone
system/domx/omx_proxy_common/src/omx_proxy_common.c:1841        OMX_ProxyCommonInit()   ERROR:  - returning error: OMX_ErrorUndefined
system/domx/omx_proxy_common/src/omx_proxy_common.c:1841        OMX_ProxyCommonInit()   ERROR: Error code: 0x80001001
system/domx/omx_proxy_common/src/omx_proxy_common.c:1841        OMX_ProxyCommonInit()   ERROR:  - Error initializing RPC
video/omx_proxy_component/src/omx_proxy_camera.c:173    OMX_ComponentInit()     ERROR: ror in Initializing Proxy
Caught SIGSEGV accessing address (nil)
#0  0x2abcafc6 in ?? ()
#1  0x2abc9c7e in ?? ()

Thank you

Marc

  • /dev/video devices are display devices. Camera on OMAP4 is available through OMX. Please check that you have Ducati firmware with camera support. Typically opensource releases do not have this. 

    You should be able to achieve video playback with opensource release using playbin2.