This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] SK-AM62: FAQ: How do I set the DIP switches to get a certain boot mode?

Part Number: SK-AM62


The AM62x SK-EVM has two 8-position DIP switches to set the SoC boot mode and related parameters. How do these switches correspond to the boot mode pins documented in the TRM?

  • You’ll need to look at the SK-EVM’s schematics in order to map the boot mode pins documented in the AM62x TRM to the DIP switches on the SK-EVM. Please follow the steps described below:

    1. The AM62x SK-EVM's schematics can be found at https://www.ti.com/tool/SK-AM62 -> Design files -> SK-AM62 Design File Package  SPRR448.ZIP (65345 KB). Download this file and unzip it, and the schematics is located at sprr448\E3 revision\Schematic\PROC114E3_SCH.pdf.

    2. Open the schematics PDF file and locate the picture below:

    3. Notice that SYS BOOTMODE0 is connected to SW1, position 1, and so on.

    4. From the TRM, locate the BOOTMODE pins tables:

    5. Now you can map the BOOTMODE pin settings provided by the TRM to the DIP switch positions on the SK-EVM, for a certain PLL clock and boot mode. For example, refer to the table below for setting the PLL clock to 25MHz and the boot mode to SD card boot:

    6. Finally the DIP switches on the SK-EVM can be physically set as shown below (note the positions of the 2 DIP switches on the board):

    Refer to the AM62x Linux Academy for more boot mode settings.