This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-J721E: CurrentRegister of PowerMonitoring PW2 is 0

Part Number: PROCESSOR-SDK-J721E

Hello.

I use J721EXCP01EVM to read data from PowerMonitoring.

PW1 is fine, but PW2's CurrentRegisters are all 0.

I think the cause is Calibration Register is 0.

What causes the PW2 calibration register to be 0?

Part of acquired data

・PW1 [VDD_MCU_0V85_REGVDD_MCU_0V85]

Configuration Register 0x4527
Shunt Voltage Register 0x0942
Bus Voltage Register  0x02ad
Power Register 0x0052
Current Register 0x0942
Calibration Register 0x0800
Mask/Enable Register  0x0008
Alert Limit Register 0x0000
Manufacturer ID Register  0x5449
Die ID Register 0x2260

・PW2 [VDD_MCUIO_1V8_REG    VDD_IO_1V8]

Configuration Register 0x4127
Shunt Voltage Register 0x0031
Bus Voltage Register  0x059d
Power Register 0x0000
Current Register 0x0000
Calibration Register 0x0000
Mask/Enable Register  0x0008
Alert Limit Register 0x0000
Manufacturer ID Register  0x5449
Die ID Register 0x2260