Are there any planned system on module implementations for the AM389x processors? If so, please advise which vendors are most likely to support this configuration. Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Are there any planned system on module implementations for the AM389x processors? If so, please advise which vendors are most likely to support this configuration. Thanks!
Z3 Technology makes a DM8168-based SOM. http://www.z3technology.com/Z3-DM368-MOD.htm
DM8168 is the exact same device as AM389x, but with added HD video accelerators and a powerful DSP. The devices are pin for pin compatible. So you could either use the DM8168-based SOM as is or talk with Z3 about making a AM389x-based SOM. The latter should be easy since the board layout would not change.