This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Support for custom C6713 in CCSv4

Hi,

I am using a custom board with TMS320C6713B DSP.

A spectrum digital XDS510 USB JTAG Emulator and CCS v4.2.3 ( 1month trial version).

I am trying to create a target configuration file in CCS.

I have selected the emulator that I am using and when I want to select the processor (C6713 B)

there is not option for such device (the only device that I can see is DSK6713).

Does this mean CCS v4 does not support any custom boards with the C6713B DSP?

Or is there something else that I need to install to setup the correct device in the configuration file?

 

Please help.

Thanks,

Aditi.