This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

build error in tms320c6713

Hi all,

I am working in tms320c6713 along with the matlab version 7.1.0.246...............i am amble to build the model via ccs3.3 but i am receiving error like this:

CCS log file indicate build incomplete...sth like this..........my project is breath signal analysis..........i am giving adc as input.......but i have not given mic to the hardware port.......so any idea y this kind of error is coming?

regards

mridula

  • Hi all,

    This is the exact kind of error message that i am getting:

    error: can't allocate .far, size 00897c40 (page 0) in IRAM (avail:
                0003fe00)
    >>   error: errors in input - mr1.out not built

    >> Compilation failure

    Build Complete,
      3 Errors, 0 Warnings, 0 Remarks.


    CCS build log file does not indicate completed build.  Please investigate.

    Please offer some help

  • Hi Mridula,

    It looks like you are having an allocation issue within your linker command file. The size of the .far allocation is bigger than the IRAM memory. Please review your linker command file.

    Thanks,

    Tai Nguyen