This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear,
we are starting our project referring to ti-processor-sdk-linux-j7-evm-08_02_00_03-Linux-x86-Install.
However, in this SDK, R5F image was loaded and started by kernel, which makes the R5F start too late.
We want to load the image by spl(tiboot3.bin) on MCU R5, right after the sysfw.itb(or A72 ATF) was installed, which will make the R5F0&1 be fast started.
Is our method available? and could you give some suggestion? Do you have any demo to realize our target?
Besides, referring to the SBL mode, the R5F would be fast started by SBL, but we didnt find the method to load the kernel image and FS.
Could you give guide on the SBL mode? what files should i put into the BOOT partition of my SD or EMMC?
thanks.
Hello,
tiboot3.bin is the first thing to be loaded which is R5F SPL. The R5F SPL loads the A72 ATF/SPL.
Are you talking about MCU domain R5Fs or the Main domain R5Fs. Even the main domain R5Fs
can be loaded by U-Boot.
Here is the detailed boot flow: software-dl.ti.com/.../UG-General-Info.html
Let me know what is you expectation.
- Keerthy
What the customer wants is that the R5F of the main domain is loaded through spl (tiboot3.bin). He wants to complete the startup of the R5F of the main domain before u-boot is loaded
That is NOT supported in the SDK & No plans to support in the future SDK as well. This is a design decision. In case customer has concerns with Main domain R5F boot timing then we recommend customer for use R5 SBL. That can load the Main domain R5F firmware.
Closing this thread.
- Keerthy
Hi,
This was the older boot flow pre 7.0 SDK. Post that we do not support loading of main domain R5 Cores from R5 SPL.
The feature was descoped after HSM re-architecture was done. So we do NOT support this as told earlier.
- Keerthy
Loading of remote cores in the new architecture is not palnned to implemented in any of the future SDKs. If that's needed then I request you to use SBL.
Closing this thread.
Best Regards,
Keerthy