This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: After TDA4VL receives RAW data and processed by isp modular, can CSIRX directly transmit data to CSITX through physical channel?

Part Number: TDA4VM

HI TI

Please help to evaluate whether the following solutions are feasible, thank you.

1.Whether the data processed by the ISP can be divided into two channels, one of which is sent to the subsequent function for sensing function. At the same time, CSIrx and csitx are directly connected through the hardware physical channel, and the data is directly transmitted from CSIRS to CSITX through the physical channel, without going through the cpu. Is this design supported?

2.Whether the ISP supports output of YUV422 format data?