Part Number: AM3358
Hi Sir
We use your AM3358 on several project. We find sometimes the our RAM/ROM test are fail (read files from eMMC and calculate the checksum). We can fix this problem by adding a small capacitor (C232) on CLK line.

This capacitor can improve the voltage dropping on CLK.

After measuring the data and CLK line looks like the voltage dropping come from the data line.

When data line pull up or pull low CLK line may have ringing.
Zoom in and check the timing.

The voltage dropping of CLK is earlier than DATA pull low. So it should not be the crosstalk from DATA line. The root cause may come from the MCU inside.
Do you have any idea that CLK have the ringing when data line change the level?
Is there any SW setting we can modify to improve the problem?
Thanks