I am planning to use the PCie adapter card for the EVMs (C6670 and C6678) to connect to a PC via PCIe. My OS is Linux PC. We need to talk to the DSP using Linux PC via the PCIe , is there a driver for a Linux PC?
Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am planning to use the PCie adapter card for the EVMs (C6670 and C6678) to connect to a PC via PCIe. My OS is Linux PC. We need to talk to the DSP using Linux PC via the PCIe , is there a driver for a Linux PC?
Regards
Hi Hector,
What PCIe adapter card are you planning to use? Is there a TI one that converts the EVM AMC card into a PCIe plug-in card?
Richard
Hi Richard,
Yes, TI has an engagement with infochip to provide a PCIe adapter card for the EVM. .
Regards,
Hector Rivera
Richard,
Here is a link for the card.
http://focus.ti.com/docs/toolsw/folders/print/tmdxevmpci.html
Regards,
Hector Rivera