This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-TDA4VM: Problem in running OProfile 1.4.0 on the board

Part Number: SK-TDA4VM


Hello,

We have compiled OProfile 1.4.0 for SK-TDA4VM. But not successful in running it on the board. It gives the following error message. Can you please help us run this profiler / give some guidance on this topic.

============================================================

root@tda4vm-sk:/opt/edge_ai_apps# operf --help
Unable to obtain cpu_type
Verify that a pre-1.0 version of OProfile is not in use.
If the /dev/oprofile/cpu_type file exists, locate the pre-1.0 OProfile
installation, and use its 'opcontrol' command, passing the --deinit option.
Unable to ascertain cpu type.  Exiting.

============================================================

Regards,

Vishwanath Kulkarni.