Other Parts Discussed in Thread: OMAP3530
Hi there,
I've been searching high and low for help on this but have reached a brick wall so to speak and am hoping someone out there can help!
I'm trying to use McBSP3 on the OMAP3530 to TX a bunch of data using the SDMA block and am having problems. I'm trying to run the example code given in
http://e2e.ti.com/support/dsp/omap_applications_processors/f/447/t/47984.aspx?PageIndex=3
specifically the TXRX example code but modified for use with McBSP3. I'm monitoring the RXBUFF1/2/3 and don't see anything changing. I noticed that the DMA_CCR14.ENABLE does not go high (ie, is not enabled) even after explicitly writing to it. It doesn't seem to like to be enabled when the MCBSPLP_SPCR2_REG.XRST is enabled?? If I do not set the XRST bit then the DMA_CCR14.ENABLE bit can be set but if XRST is enabled then it doesn't seem like I can set the DMA ENABLE bit. I checked the CSR register and don't see anything out of the ordinary.
I'm running this on Angstrom Linux but have modified the example code to support that. The TXRX code is below. I also had to 'fix' the original sample file mcbsp_lib.c/mcbspEnableFclk and mcbspEnableIClk --> SETBIT_REGL selects the wrong MCBSPs for MCBSP3 and MCBSP4.
I'm sure that I'm doing something stupid but I can't seem to figure it out....
Thanks in advance for any help.
Robin
-------
#include "MCBSP.h"
#include "PRCM.h"
#include "CONTROL.h"
#include "operations.h"
#include "mcbsp_lib.h"
#include "DMA.h"
#include "dma_lib.h"
#include <stdio.h>
#define MY_MCBSP MCBSP3
int main (void)
{
unsigned int loop;
unsigned int read_data, read_data2;
unsigned int RXBUFF1[16] = {0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0};
unsigned int RXBUFF2[16] = {0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0};
unsigned int RXBUFF3[16] = {0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0};
unsigned int TXBUFF1[16] = {0x1f,0x1e,0x1d,0x1c,0x1b,0x1a,0x19,0x18,0x17,0x16,0x15,0x14,0x13,0x12,0x11,0x10};
unsigned int TXBUFF2[16] = {0x20,0x21,0x22,0x23,0x24,0x25,0x26,0x27,0x28,0x29,0x2A,0x2B,0x2C,0x2D,0x2E,0x2F};
unsigned int allrxbuff[3] = {(unsigned int)&RXBUFF1[0], (unsigned int)&RXBUFF2[0], (unsigned int)&RXBUFF3[0]};
unsigned int alltxbuff[2] = {(unsigned int)&TXBUFF1[0], (unsigned int)&TXBUFF2[0]};
unsigned int i, j;
// Setup the RX DMA - 3 buffers
dmaSetCsdp(CHAN11, SRC_LITTLE_ENDIAN, SRC_ENDIAN_ADAPT, DST_LITTLE_ENDIAN, DST_ENDIAN_ADAPT,
WRITE_POSTED, DST_NO_BURST, DST_UNPACKED, SRC_NO_BURST, SRC_UNPACKED, SCALAR_32BITS);
dmaSetCsdp(CHAN12, SRC_LITTLE_ENDIAN, SRC_ENDIAN_ADAPT, DST_LITTLE_ENDIAN, DST_ENDIAN_ADAPT,
WRITE_POSTED, DST_NO_BURST, DST_UNPACKED, SRC_NO_BURST, SRC_UNPACKED, SCALAR_32BITS);
dmaSetCsdp(CHAN13, SRC_LITTLE_ENDIAN, SRC_ENDIAN_ADAPT, DST_LITTLE_ENDIAN, DST_ENDIAN_ADAPT,
WRITE_POSTED, DST_NO_BURST, DST_UNPACKED, SRC_NO_BURST, SRC_UNPACKED, SCALAR_32BITS);
dmaSetCcr(CHAN11, LOW_WR_PRIORITY, EN_BUFF, TRG_SRC, NO_PREFETCH, DIS_SUPER, DIS_TRANS_COPY, DIS_CONST_FILL,
DST_AMODE_POST_INC, SRC_AMODE_CONST, DIS_SUSPEND, DIS_CHANNEL, LOW_RD_PRIORITY, TRANS_FRAME, DMA_MCBSP3_DMA_RX );
dmaSetCcr(CHAN12, LOW_WR_PRIORITY, EN_BUFF, TRG_SRC, NO_PREFETCH, DIS_SUPER, DIS_TRANS_COPY, DIS_CONST_FILL,
DST_AMODE_POST_INC, SRC_AMODE_CONST, DIS_SUSPEND, DIS_CHANNEL, LOW_RD_PRIORITY, TRANS_FRAME, DMA_MCBSP3_DMA_RX );
dmaSetCcr(CHAN13, LOW_WR_PRIORITY, EN_BUFF, TRG_SRC, NO_PREFETCH, DIS_SUPER, DIS_TRANS_COPY, DIS_CONST_FILL,
DST_AMODE_POST_INC, SRC_AMODE_CONST, DIS_SUSPEND, DIS_CHANNEL, LOW_RD_PRIORITY, TRANS_FRAME, DMA_MCBSP3_DMA_RX );
dmaConfigTransfer(CHAN11, 16, 1, (MY_MCBSP+MCBSPLP_DRR_REG), (unsigned int)RXBUFF1, 1, 0, 1, 0);
dmaConfigTransfer(CHAN12, 16, 1, (MY_MCBSP+MCBSPLP_DRR_REG), (unsigned int)RXBUFF2, 1, 0, 1, 0);
dmaConfigTransfer(CHAN13, 16, 1, (MY_MCBSP+MCBSPLP_DRR_REG), (unsigned int)RXBUFF3, 1, 0, 1, 0);
dmaSetChannelLink(CHAN11, CHAN12, EN_CHAN_LINK);
dmaSetChannelLink(CHAN12, CHAN13, EN_CHAN_LINK);
dmaSetChannelLink(CHAN13, CHAN11, EN_CHAN_LINK);
dmaEnableChannel(CHAN11);
// Setup the TX DMA - 2 buffers
dmaSetCsdp(CHAN14, SRC_LITTLE_ENDIAN, SRC_ENDIAN_ADAPT, DST_LITTLE_ENDIAN, DST_ENDIAN_ADAPT,
WRITE_POSTED, DST_NO_BURST, DST_UNPACKED, SRC_NO_BURST, SRC_UNPACKED, SCALAR_32BITS);
dmaSetCcr(CHAN14, LOW_WR_PRIORITY, EN_BUFF, TRG_DEST, NO_PREFETCH, DIS_SUPER, DIS_TRANS_COPY, DIS_CONST_FILL,
DST_AMODE_CONST, SRC_AMODE_POST_INC, DIS_SUSPEND, DIS_CHANNEL, LOW_RD_PRIORITY, TRANS_FRAME, DMA_MCBSP3_DMA_TX );
dmaConfigTransfer(CHAN14, 16, 1, (unsigned int)TXBUFF1, (MY_MCBSP+MCBSPLP_DXR_REG), 1, 0, 1, 0);
dmaSetChannelLink(CHAN14, CHAN15, EN_CHAN_LINK);
dmaSetCsdp(CHAN15, SRC_LITTLE_ENDIAN, SRC_ENDIAN_ADAPT, DST_LITTLE_ENDIAN, DST_ENDIAN_ADAPT,
WRITE_POSTED, DST_NO_BURST, DST_UNPACKED, SRC_NO_BURST, SRC_UNPACKED, SCALAR_32BITS);
dmaSetCcr(CHAN15, LOW_WR_PRIORITY, EN_BUFF, TRG_DEST, NO_PREFETCH, DIS_SUPER, DIS_TRANS_COPY, DIS_CONST_FILL,
DST_AMODE_CONST, SRC_AMODE_POST_INC, DIS_SUSPEND, DIS_CHANNEL, LOW_RD_PRIORITY, TRANS_FRAME, DMA_MCBSP3_DMA_TX );
dmaConfigTransfer(CHAN15, 16, 1, (unsigned int)TXBUFF2, (MY_MCBSP+MCBSPLP_DXR_REG), 1, 0, 1, 0);
// For this example, disable the automatic linking of channel 15 to channel 14 so that it will be easier to set a breakpoint
// and view the changes to the RX buffers. Channel 14 will be enabled later as part of a continuious loop.
//dmaSetChannelLink(CHAN15, CHAN14, EN_CHAN_LINK);
//dmaEnableChannel(CHAN14);
/////////////////////////////////////////////////////////////
// Select clock sources and switch on Switch on the clocks
cmEnableClock96M();
mcbspEnableIclk(MY_MCBSP);
mcbspSelectClksSource(MY_MCBSP, INTERNAL_FCLK);
mcbspEnableFclk(MY_MCBSP);
mcbspSet4Pin(MY_MCBSP); // Sets McBSP1 to 4 pin mode.
/////////////////////////////////////////////////////////////
// reset module
mcbspReset(MY_MCBSP, 1);
/////////////////////////////////////////////////////////////
// Configure transmitter and receiver
mcbspSetRxMode(MY_MCBSP, CLK_EXTERNAL, CLKR_SAMPLE_FALL, SYNC_EXTERNAL, SYNC_ACTIVE_HIGH, FULL_CYCLE);
mcbspSetTxMode(MY_MCBSP, CLK_INTERNAL, CLKX_DRIVE_RISE, SYNC_INTERNAL, SYNC_ACTIVE_HIGH, HALF_CYCLE, DXENA_OFF, XCLK_FREE, FSX_GATED);
/////////////////////////////////////////////////////////////
// Set up frames
mcbspRxFrameSetup(MY_MCBSP, SINGLE_PHASE, MSB_FIRST, DELAY_0BIT, 4, WORD_8BITS, 1, WORD_8BITS, RIGHT_JUST_ZERO);
mcbspTxFrameSetup(MY_MCBSP, SINGLE_PHASE, MSB_FIRST, DELAY_0BIT, 4, WORD_8BITS, 1, WORD_8BITS);
/////////////////////////////////////////////////////////////
// Program the Sample Rate generator
mcbspSetupSrg(MY_MCBSP, CLKS, CLKS_RISE, SRG_FREE, 32, 8, 255);
/////////////////////////////////////////////////////////////
// Configure the loopback
mcbspLoopback(MY_MCBSP, DIGITAL_LOOPBACK);
/////////////////////////////////////////////////////////////
// Set the buffer thresholds
mcbspSetRxThresh(MY_MCBSP, 16);
mcbspSetTxThresh(MY_MCBSP, 16);
mcbspEnableTxDma(MY_MCBSP);
mcbspEnableRxDma(MY_MCBSP);
/////////////////////////////////////////////////////////////
// Delay to allow settings to sync
//
for (loop=0; loop <0XFF; loop++);
/////////////////////////////////////////////////////////////
// Configure the pins
//
OUT_REGL(CONTROL_PADCONF_MCBSP3_CLKX, 0x01080108); // 31:16 = mcbsp1_fsr 15:0 = mcbsp1_clkr
OUT_REGL(CONTROL_PADCONF_MCBSP3_DX, 0x01080008); // 31:16 = mcbsp1_dr 15:0 = mcbsp1_dx
/////////////////////////////////////////////////////////////
// Remove Resets
mcbspRemoveResetSrg(MY_MCBSP);
mcbspRemoveResetFsg(MY_MCBSP);
mcbspRemoveResetRx(MY_MCBSP);
mcbspRemoveResetTx(MY_MCBSP);
// For each breakpoint halt you can observe 2 of the 3 RX buffers update with the TX data.
// The RX buffer updates will cycle through all 3 buffers.
while (1) {
read_data2 = IN_REGL(DMA_CSRi + (CHAN14 * 0x60));
read_data = IN_REGL(DMA_CCRi + (CHAN14 * 0x60));
dmaEnableChannel(CHAN14);
printf("reg value is 0x%x (CSR = 0x%x)\n", (unsigned int)read_data, (unsigned int)read_data2);
for (loop=0; loop <0XF; loop++)
{
printf("**************\n\n");
// Set breakpoint here
for (i=0; i<=2; i++)
{
for (j=0; j<=15; j++)
{
printf("RXBUFF%d[%d] = 0x%x\n", i, j, ((unsigned int *)allrxbuff[i])[j]);
}
printf("-----------\n");
}
/*
printf("-----------\n");
for (i=0; i<=1; i++)
{
for (j=0; j<=15; j++)
{
printf("TXBUFF%d[%d] = 0x%x\n", i, j, ((unsigned int *)alltxbuff[i])[j]);
}
}
getchar();
*/
}
}
}