This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Want to ask how should the system adapt to make SDL work properly in SPL mode?

Part Number: TDA4VM

Hi Expers,

We wanted to integrate SDL on the project, and now we are encountering a lot of problems with the integration. I see that all of SDL's test cases are validated based on SBL boot mode. Currently we use SPL mode, SDL many test cases can not pass. Want to ask how should the system adapt to make SDL work properly in SPL mode?
Thank you!

  • Hi,

    The Software Diagnostics Library from TI, as of SDK 8.2, is only validated on the SBL boot flow.   

    Yes it is likely possible to implement SDL in SPL boot mode, however TI does not currently have an example of this for SDK8.2, or for the upcoming SDK 8.4 release, that I am aware of.

    Regards,

    kb