Other Parts Discussed in Thread: DRA829
Hi Team,
I received a question from my customer regarding the QSGMII pins. Which of the following combinations is the correct pin combination they should use? Also, are there any restrictions such that it will prevent other pin usage?
- SERDES0_TX0_P/SGMII1_TXP0, SERDES0_TX0_N/SGMII1_TXN0, SERDES0_RX0_P/SGMII1_RXP0, SERDES0_RX0_N/SGMII1_RXN0
- SERDES0_TX1_P/SGMII2_TXP0, SERDES0_TX1_N/SGMII2_TXN0, SERDES0_RX1_P/SGMII2_RXP0, SERDES0_RX1_N/SGMII2_RXN0
- SERDES1_TX0_P/SGMII3_TXP0, SERDES1_TX0_N/SGMII3_TXN0, SERDES1_RX0_P/SGMII3_RXP0, SERDES1_RX0_N/SGMII3_RXN0
- SERDES1_TX1_P/SGMII4_TXP0, SERDES1_TX1_N/SGMII4_TXN0, SERDES1_RX1_P/SGMII4_RXP0, SERDES1_RX1_N/SGMII4_RXN0
Also in the datasheet(SPRSP35J)p1, it says "Up to two QSGMII", so their understanding is that there are 2 channels. However, in the TRM(SPRUIL1C)p1874, it seems from Table 12-259 and Table 12-260 that there are 4 channels like the ones above.
Also the EVM uses the combination #2 above correct? They will be using a different SERDES, so they presume they will use combination #4, and have no plans of using #1 and #2. If they connect it as SGMII, will there be no issues? In the QSGMII Specification Revision 1.3, EDCS-540123, it says that QSGMII is defined as four SGMII interleaved with a single link with a 4-channel selector and 2-bit free counter, but they are concerned that using one QSGMII may not function as a SGMII x4ch.
Best regards,
Mari Tsunoda