Part Number: AM3352
Other Parts Discussed in Thread: ADS7846, BQ24190, TWL6040, DRA752, TPS65023, TPS62360, TPS65218, BQ24735, TMP102, TPS65217, TSC2005, TPS65910, TSC2007
I get the following error on ti-linux-kernel v08.04.01.002 (based on v5.10.136) compiled with no modifications beyond my defconfig and dts. The hardware is an Olimex AM3352-SOM which is very similar to the EVM design.
[ 154.843094] omap_intc_handle_irq: spurious irq! [ 154.850046] ============================= [ 154.850064] WARNING: suspicious RCU usage [ 154.850082] 5.10.136-00001-geeddd634953 #9 Not tainted [ 154.850099] ----------------------------- [ 154.850118] ./include/trace/events/lock.h:37 suspicious rcu_dereference_check() usage! [ 154.850148] other info that might help us debug this: [ 154.850191] rcu_scheduler_active = 2, debug_locks = 1 [ 154.850209] RCU used illegally from extended quiescent state! [ 154.850225] no locks held by swapper/0/0. [ 154.850253] stack backtrace: [ 154.850272] CPU: 0 PID: 0 Comm: swapper/0 Not tainted 5.10.136-00001-geeddd634953 #9 [ 154.850289] Hardware name: Generic AM33XX (Flattened Device Tree) [ 154.850308] [<c01110c8>] (unwind_backtrace) from [<c010c118>] (show_stack+0x10/0x14) [ 154.850326] [<c010c118>] (show_stack) from [<c0a4ff48>] (dump_stack+0xe0/0x10c) [ 154.850344] [<c0a4ff48>] (dump_stack) from [<c01affc8>] (lock_acquire+0x304/0x444) [ 154.850363] [<c01affc8>] (lock_acquire) from [<c0a5d270>] (_raw_spin_lock+0x40/0x50) [ 154.850382] [<c0a5d270>] (_raw_spin_lock) from [<c01bc808>] (vprintk_emit+0x5c/0x2dc) [ 154.850400] [<c01bc808>] (vprintk_emit) from [<c01bcaa8>] (vprintk_default+0x20/0x28) [ 154.850418] [<c01bcaa8>] (vprintk_default) from [<c0a4c94c>] (printk+0x2c/0x54) [ 154.850436] [<c0a4c94c>] (printk) from [<c0643128>] (omap_intc_handle_irq+0x74/0x90) [ 154.850456] [<c0643128>] (omap_intc_handle_irq) from [<c0100b70>] (__irq_svc+0x70/0x98) [ 154.850472] Exception stack(0xc1001f10 to 0xc1001f58) [ 154.850491] 1f00: ffffffff ffffffff 00000001 c011c3a0 [ 154.850510] 1f20: c1109ce0 c1009254 00000001 c100929c 00000000 00000000 c1009208 c10092b4 [ 154.850527] 1f40: c1000000 c1001f60 c0108634 c0108638 60010013 ffffffff [ 154.850546] [<c0100b70>] (__irq_svc) from [<c0108638>] (arch_cpu_idle+0x30/0x3c) [ 154.850564] [<c0108638>] (arch_cpu_idle) from [<c0a5cff0>] (default_idle_call+0x78/0x2b8) [ 154.850583] [<c0a5cff0>] (default_idle_call) from [<c017b548>] (do_idle+0x1d4/0x2b4) [ 154.850601] [<c017b548>] (do_idle) from [<c017b9fc>] (cpu_startup_entry+0x18/0x1c) [ 154.850620] [<c017b9fc>] (cpu_startup_entry) from [<c0f00f68>] (start_kernel+0x488/0x568)
dts:
/*
* Copyright (C) 2012 Texas Instruments Incorporated - http://www.ti.com/
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
* published by the Free Software Foundation.
*/
/dts-v1/;
#include "am33xx.dtsi"
#include <dt-bindings/pwm/pwm.h>
#include <dt-bindings/interrupt-controller/irq.h>
/ {
model = "OLIMEX AM335x-SOM VoltServer ETX8";
compatible = "olimex,am335x_som", "ti,am33xx";
chosen {
stdout-path = &uart0;
tick-timer = &timer2;
};
leds: leds {
compatible = "gpio-leds";
};
gpio_keys: gpio_keys {
compatible = "gpio-keys";
};
memory {
device_type = "memory";
reg = <0x80000000 0x20000000>; /* 512 MB */
};
dummy_reg: regulator@0 {
compatible = "regulator-fixed";
regulator-name = "dummy_regulator";
regulator-min-microvolt = <3300000>;
regulator-max-microvolt = <3300000>;
};
};
&leds {
pinctrl-names = "default";
pinctrl-0 = <&usr_led_pins_default>, <&evb_leds_pins_default>;
led@0 {
label = "olimex-som:green:led1";
gpios = <&gpio3 18 GPIO_ACTIVE_HIGH>;
linux,default-trigger = "heartbeat";
default-state = "off";
};
led@1 {
label = "etx8:blue:led2"; // red on the Olimex EVB
gpios = <&gpio3 20 GPIO_ACTIVE_HIGH>;
linux,default-trigger = "none"; // "mmc0"
default-state = "off";
};
led@2 {
label = "etx8:green:led3"; // yellow on the Olimex EVB
gpios = <&gpio3 21 GPIO_ACTIVE_HIGH>;
linux,default-trigger = "heartbeat"; // "cpu0"
default-state = "off";
};
};
&am33xx_pinmux {
usr_led_pins_default: usr_led_pins_default {
pinctrl-single,pins = <
AM33XX_PADCONF(AM335X_PIN_MCASP0_ACLKR, PIN_OUTPUT, MUX_MODE7) /* (B12) gpio3_18 */
/* 0x1a0 ( PIN_OUTPUT | MUX_MODE7 ) /* (B12) mcasp0_aclkr.gpio3_18 */
>;
};
evb_leds_pins_default: evb_leds_pins_default {
pinctrl-single,pins = <
AM33XX_PADCONF(AM335X_PIN_MCASP0_AXR1, PIN_OUTPUT, MUX_MODE7) /* (D13) mcasp0_axr1.gpio3_20 */
AM33XX_PADCONF(AM335X_PIN_MCASP0_AHCLKX, PIN_OUTPUT, MUX_MODE7) /* (A14) mcasp0_ahclkx.gpio3_21 */
/* 0x1a8 ( PIN_OUTPUT | MUX_MODE7 ) /* (D13) mcasp0_axr1.gpio3_20 */
/* 0x1ac ( PIN_OUTPUT | MUX_MODE7 ) /* (A14) mcasp0_ahclkx.gpio3_21 */
>;
};
};
&gpio_keys {
label = "gpio keys";
factory_reset {
label = "Factory RESET";
linux,code = <87>; /* F11 key */
gpios = <&gpio3 19 GPIO_ACTIVE_LOW>; // pin 35 on AM_CON-LCD header
/* Note: dmesg will show an error "omap_gpio 44e07000.gpio: Could not set line 19 debounce to 50000 microseconds (-22)"
However the gpio-keys driver will use software debounce instead. The max hw debounce is 7.9 ms */
debounce-interval = <50>;
};
};
&am33xx_pinmux {
pinctrl-0 = <&gpio3_pins>;
gpio3_pins: pinmux_gpio3_pins {
pinctrl-single,pins = <
AM33XX_PADCONF(AM335X_PIN_MCASP0_FSR, PIN_INPUT_PULLUP, MUX_MODE7) /* (C13) gpio3_19 */
/* 0x1e4 (PIN_INPUT_PULLUP | MUX_MODE7) /* (C13) emu0.gpio3_19 */
/*0x1e4 (PIN_INPUT_PULLUP | MUX_MODE7) /* (C14) emu0.gpio3_7 */
/*0x1e8 (PIN_INPUT_PULLUP | MUX_MODE7) /* (B14) emu1.gpio3_8 */
>;
};
};
&uart0 {
pinctrl-names = "default";
pinctrl-0 = <&uart0_pins>;
status = "okay";
};
&am33xx_pinmux {
uart0_pins: uart0_pins_default {
pinctrl-single,pins = <
AM33XX_PADCONF(AM335X_PIN_UART0_RXD, PIN_INPUT_PULLUP, MUX_MODE0)
AM33XX_PADCONF(AM335X_PIN_UART0_TXD, PIN_OUTPUT_PULLDOWN, MUX_MODE0)
>;
};
};
&uart1 {
pinctrl-names = "default";
pinctrl-0 = <&uart1_pins>;
status = "okay";
};
&am33xx_pinmux {
uart1_pins: pinmux_uart1_pins {
pinctrl-single,pins = <
AM33XX_PADCONF(AM335X_PIN_UART1_RXD, PIN_INPUT_PULLUP, MUX_MODE0)
AM33XX_PADCONF(AM335X_PIN_UART1_TXD, PIN_OUTPUT_PULLDOWN, MUX_MODE0)
>;
};
};
&uart4 {
pinctrl-names = "default";
pinctrl-0 = <&uart4_pins>;
status = "disabled";
};
&am33xx_pinmux {
uart4_pins: pinmux_uart4_pins {
pinctrl-single,pins = <
AM33XX_PADCONF(AM335X_PIN_UART0_CTSN, PIN_INPUT_PULLUP, MUX_MODE1) /* (E18) uart0_ctsn.uart4_rxd */
AM33XX_PADCONF(AM335X_PIN_UART0_RTSN, PIN_OUTPUT, MUX_MODE1) /* (E17) uart0_rtsn.uart4_txd */
/* 0x168 ( PIN_INPUT_PULLUP | MUX_MODE1 ) /* (E18) uart0_ctsn.uart4_rxd */
/* 0x16c ( PIN_OUTPUT | MUX_MODE1 ) /* (E17) uart0_rtsn.uart4_txd */
>;
};
};
&mmc1 {
status = "okay";
bus-width = <0x4>;
pinctrl-names = "default";
pinctrl-0 = <&mmc1_pins>;
cd-gpios = <&gpio0 6 GPIO_ACTIVE_HIGH>;
cd-inverted;
vmmc-supply = <&dummy_reg>;
};
&am33xx_pinmux {
mmc1_pins: pinmux_mmc1_pins {
pinctrl-single,pins = <
AM33XX_PADCONF(AM335X_PIN_SPI0_CS1, PIN_INPUT, MUX_MODE7) /* spi0_cs1.gpio0_6 */
AM33XX_PADCONF(AM335X_PIN_MMC0_DAT0, PIN_INPUT_PULLUP, MUX_MODE0)
AM33XX_PADCONF(AM335X_PIN_MMC0_DAT1, PIN_INPUT_PULLUP, MUX_MODE0)
AM33XX_PADCONF(AM335X_PIN_MMC0_DAT2, PIN_INPUT_PULLUP, MUX_MODE0)
AM33XX_PADCONF(AM335X_PIN_MMC0_DAT3, PIN_INPUT_PULLUP, MUX_MODE0)
AM33XX_PADCONF(AM335X_PIN_MMC0_CMD, PIN_INPUT_PULLUP, MUX_MODE0)
AM33XX_PADCONF(AM335X_PIN_MMC0_CLK, PIN_INPUT_PULLUP, MUX_MODE0)
>;
};
};
&mac {
pinctrl-names = "default";
pinctrl-0 = <&cpsw1_pins>; /*, <&cpsw2_pins>; */
status = "okay";
/* dual_emac = <1>; */
slaves = <1>;
};
&am33xx_pinmux {
/* Refer to LAN8710A 00002164B.pdf table 2-1, p7 */
cpsw1_pins: pinmux_cpsw1 {
pinctrl-single,pins = <
AM33XX_PADCONF(AM335X_PIN_MII1_TX_EN, PIN_OUTPUT_PULLDOWN, MUX_MODE0) /* mii1_txen.rgmii1_tctl */
AM33XX_PADCONF(AM335X_PIN_MII1_RX_DV, PIN_INPUT_PULLUP, MUX_MODE0) /* mii1_rxdv.rgmii1_rctl */
AM33XX_PADCONF(AM335X_PIN_MII1_TXD3, PIN_OUTPUT_PULLDOWN, MUX_MODE0) /* mii1_txd3.rgmii1_td3 */
AM33XX_PADCONF(AM335X_PIN_MII1_TXD2, PIN_OUTPUT_PULLDOWN, MUX_MODE0) /* mii1_txd2.rgmii1_td2 */
AM33XX_PADCONF(AM335X_PIN_MII1_TXD1, PIN_OUTPUT_PULLDOWN, MUX_MODE0) /* mii1_txd1.rgmii1_td1 */
AM33XX_PADCONF(AM335X_PIN_MII1_TXD0, PIN_OUTPUT_PULLDOWN, MUX_MODE0) /* mii1_txd0.rgmii1_td0 */
AM33XX_PADCONF(AM335X_PIN_MII1_TX_CLK, PIN_INPUT_PULLUP, MUX_MODE0) /* mii1_txclk.rgmii1_tclk */
AM33XX_PADCONF(AM335X_PIN_MII1_RX_CLK, PIN_INPUT_PULLUP, MUX_MODE0) /* mii1_rxclk.rgmii1_rclk */
AM33XX_PADCONF(AM335X_PIN_MII1_RXD3, PIN_INPUT_PULLUP, MUX_MODE0) /* mii1_rxd3.rgmii1_rd3 */
AM33XX_PADCONF(AM335X_PIN_MII1_RXD2, PIN_INPUT_PULLUP, MUX_MODE0) /* mii1_rxd2.rgmii1_rd2 */
AM33XX_PADCONF(AM335X_PIN_MII1_RXD1, PIN_INPUT_PULLUP, MUX_MODE0) /* mii1_rxd1.rgmii1_rd1 */
AM33XX_PADCONF(AM335X_PIN_MII1_RXD0, PIN_INPUT_PULLUP, MUX_MODE0) /* mii1_rxd0.rgmii1_rd0 */
AM33XX_PADCONF(AM335X_PIN_MII1_RX_ER, PIN_INPUT_PULLUP, MUX_MODE0) /* (J15) gmii1_rxer.gmii1_rxer */
AM33XX_PADCONF(AM335X_PIN_MII1_COL, PIN_INPUT, MUX_MODE0) /* (H16) mii1_col.gpio3_0 */
AM33XX_PADCONF(AM335X_PIN_MII1_CRS, PIN_INPUT_PULLDOWN, MUX_MODE0) /* (H17) gmii1_crs.gmii1_crs */
>;
};
cpsw2_pins: pinmux_cpsw2 {
pinctrl-single,pins = <
/* 0x78 ( PIN_INPUT | MUX_MODE1 ) /* (U18) gpmc_be1n.gmii2_col */
/* 0x70 ( PIN_INPUT | MUX_MODE1 ) /* (T17) gpmc_wait0.gmii2_crs */
/* 0x74 ( PIN_INPUT_PULLUP | MUX_MODE1 ) /* (U17) gpmc_wpn.gmii2_rxer */
AM33XX_PADCONF(AM335X_PIN_GPMC_BEN1, PIN_INPUT, MUX_MODE1) /* (U18) gpmc_be1n.gmii2_col */
AM33XX_PADCONF(AM335X_PIN_GPMC_WAIT0, PIN_INPUT, MUX_MODE1) /* (T17) gpmc_wait0.gmii2_crs */
AM33XX_PADCONF(AM335X_PIN_GPMC_WPN, PIN_INPUT_PULLUP, MUX_MODE1) /* (U17) gpmc_wpn.gmii2_rxer */
AM33XX_PADCONF(AM335X_PIN_GPMC_A0, PIN_OUTPUT_PULLDOWN, MUX_MODE1) /* gpmc_a0.rgmii2_tctl */
AM33XX_PADCONF(AM335X_PIN_GPMC_A1, PIN_INPUT_PULLDOWN, MUX_MODE1) /* gpmc_a1.rgmii2_rctl */
AM33XX_PADCONF(AM335X_PIN_GPMC_A2, PIN_OUTPUT_PULLDOWN, MUX_MODE1) /* gpmc_a2.rgmii2_td3 */
AM33XX_PADCONF(AM335X_PIN_GPMC_A3, PIN_OUTPUT_PULLDOWN, MUX_MODE1) /* gpmc_a3.rgmii2_td2 */
AM33XX_PADCONF(AM335X_PIN_GPMC_A4, PIN_OUTPUT_PULLDOWN, MUX_MODE1) /* gpmc_a4.rgmii2_td1 */
AM33XX_PADCONF(AM335X_PIN_GPMC_A5, PIN_OUTPUT_PULLDOWN, MUX_MODE1) /* gpmc_a5.rgmii2_td0 */
AM33XX_PADCONF(AM335X_PIN_GPMC_A6, PIN_OUTPUT_PULLDOWN, MUX_MODE1) /* gpmc_a6.rgmii2_tclk */
AM33XX_PADCONF(AM335X_PIN_GPMC_A7, PIN_INPUT_PULLDOWN, MUX_MODE1) /* gpmc_a7.rgmii2_rclk */
AM33XX_PADCONF(AM335X_PIN_GPMC_A8, PIN_INPUT_PULLDOWN, MUX_MODE1) /* gpmc_a8.rgmii2_rd3 */
AM33XX_PADCONF(AM335X_PIN_GPMC_A9, PIN_INPUT_PULLDOWN, MUX_MODE1) /* gpmc_a9.rgmii2_rd2 */
AM33XX_PADCONF(AM335X_PIN_GPMC_A10, PIN_INPUT_PULLDOWN, MUX_MODE1) /* gpmc_a10.rgmii2_rd1 */
AM33XX_PADCONF(AM335X_PIN_GPMC_A11, PIN_INPUT_PULLDOWN, MUX_MODE1) /* gpmc_a11.rgmii2_rd0 */
>;
};
};
&davinci_mdio {
pinctrl-names = "default"; //, "sleep";
pinctrl-0 = <&davinci_mdio_pins>;
status = "okay";
reset-gpios = <&gpio0 29 GPIO_ACTIVE_LOW>;
reset-delay-us = <25000>; /* LAN8710A 00002164B.pdf table 5-7, p60 */
ethphy0: ethernet-phy@0 {
reg = <0>;
};
/*
ethphy1: ethernet-phy@1 {
reg = <1>;
};
*/
};
&am33xx_pinmux {
/* Refer to LAN8710A 00002164B.pdf table 2-3, p12 */
davinci_mdio_pins: pinmux_davinci_mdio {
pinctrl-single,pins = <
AM33XX_PADCONF(AM335X_PIN_MDIO, PIN_INPUT_PULLUP | SLEWCTRL_FAST, MUX_MODE0)
AM33XX_PADCONF(AM335X_PIN_MDC, PIN_OUTPUT_PULLUP, MUX_MODE0)
AM33XX_PADCONF(AM335X_PIN_RMII1_REF_CLK, PIN_INPUT_PULLUP, MUX_MODE7) /* rmii2_refclk.gpio0_29 */
>;
};
};
&cpsw_emac0 {
phy-handle = <ðphy0>;
phy-mode = "mii";
/* dual_emac_res_vlan = <1>; */
};
/*
&cpsw_emac1 {
phy-handle = <ðphy1>;
phy-mode = "mii";
dual_emac_res_vlan = <2>;
};
*/
&sham {
status = "okay";
};
&aes {
status = "okay";
};
&rtc {
clocks = <&clk_32768_ck>, <&clk_24mhz_clkctrl AM3_CLK_24MHZ_CLKDIV32K_CLKCTRL 0>;
clock-names = "ext-clk", "int-clk";
};
defconfig:
CONFIG_KERNEL_LZO=y CONFIG_DEFAULT_HOSTNAME="etx8" CONFIG_SYSVIPC=y CONFIG_POSIX_MQUEUE=y CONFIG_AUDIT=y CONFIG_NO_HZ=y CONFIG_HIGH_RES_TIMERS=y CONFIG_BSD_PROCESS_ACCT=y CONFIG_IKCONFIG=y CONFIG_IKCONFIG_PROC=y CONFIG_LOG_BUF_SHIFT=16 CONFIG_CGROUPS=y CONFIG_MEMCG=y CONFIG_BLK_CGROUP=y CONFIG_CGROUP_SCHED=y CONFIG_CFS_BANDWIDTH=y CONFIG_RT_GROUP_SCHED=y CONFIG_CGROUP_FREEZER=y CONFIG_CPUSETS=y CONFIG_CGROUP_DEVICE=y CONFIG_CGROUP_CPUACCT=y CONFIG_CGROUP_PERF=y CONFIG_NAMESPACES=y CONFIG_BLK_DEV_INITRD=y CONFIG_EXPERT=y # CONFIG_COMPAT_BRK is not set CONFIG_SLAB=y CONFIG_PROFILING=y CONFIG_ARCH_MULTI_V6=y CONFIG_POWER_AVS_OMAP=y CONFIG_POWER_AVS_OMAP_CLASS3=y CONFIG_OMAP_RESET_CLOCKS=y CONFIG_ARCH_OMAP2=y CONFIG_ARCH_OMAP3=y CONFIG_ARCH_OMAP4=y CONFIG_SOC_OMAP5=y CONFIG_SOC_AM33XX=y CONFIG_SOC_AM43XX=y CONFIG_SOC_DRA7XX=y CONFIG_ARM_THUMBEE=y CONFIG_ARM_ERRATA_411920=y CONFIG_SMP=y CONFIG_NR_CPUS=2 CONFIG_ARM_APPENDED_DTB=y CONFIG_ARM_ATAG_DTB_COMPAT=y CONFIG_CMDLINE="root=/dev/mmcblk0p1 rootwait console=ttyS0,115200" CONFIG_KEXEC=y CONFIG_CPU_FREQ=y CONFIG_CPU_FREQ_DEFAULT_GOV_ONDEMAND=y CONFIG_CPU_FREQ_GOV_POWERSAVE=y CONFIG_CPU_FREQ_GOV_USERSPACE=y CONFIG_CPU_FREQ_GOV_CONSERVATIVE=y CONFIG_CPUFREQ_DT=m CONFIG_CPU_IDLE=y CONFIG_KERNEL_MODE_NEON=y CONFIG_PM_DEBUG=y CONFIG_CRYPTO_SHA1_ARM_NEON=m CONFIG_CRYPTO_SHA256_ARM=m CONFIG_CRYPTO_SHA512_ARM=m CONFIG_CRYPTO_AES_ARM=m CONFIG_CRYPTO_AES_ARM_BS=m CONFIG_CRYPTO_CRC32_ARM_CE=m CONFIG_OPROFILE=y CONFIG_KPROBES=y CONFIG_MODULES=y CONFIG_MODULE_FORCE_LOAD=y CONFIG_MODULE_UNLOAD=y CONFIG_MODULE_FORCE_UNLOAD=y CONFIG_MODVERSIONS=y CONFIG_MODULE_SRCVERSION_ALL=y # CONFIG_BLK_DEV_BSG is not set CONFIG_PARTITION_ADVANCED=y CONFIG_BINFMT_MISC=y CONFIG_CMA=y CONFIG_NET=y CONFIG_PACKET=y CONFIG_UNIX=y CONFIG_XFRM_USER=y CONFIG_NET_KEY=y CONFIG_NET_KEY_MIGRATE=y CONFIG_INET=y CONFIG_IP_MULTICAST=y CONFIG_IP_PNP=y CONFIG_IP_PNP_DHCP=y CONFIG_IP_PNP_BOOTP=y CONFIG_IP_PNP_RARP=y CONFIG_NET_IPIP=m CONFIG_NETFILTER=y CONFIG_NETFILTER_NETLINK_LOG=m CONFIG_NF_CONNTRACK=m CONFIG_NF_CONNTRACK_ZONES=y # CONFIG_NF_CONNTRACK_PROCFS is not set CONFIG_NF_CONNTRACK_EVENTS=y CONFIG_NF_CONNTRACK_TIMEOUT=y CONFIG_NF_CONNTRACK_TIMESTAMP=y CONFIG_NF_CONNTRACK_SNMP=m CONFIG_NF_CT_NETLINK=m CONFIG_NF_CT_NETLINK_TIMEOUT=m CONFIG_NETFILTER_NETLINK_GLUE_CT=y CONFIG_NF_TABLES=m CONFIG_NF_TABLES_INET=y CONFIG_NF_TABLES_NETDEV=y CONFIG_NFT_CT=m CONFIG_NFT_COUNTER=m CONFIG_NFT_CONNLIMIT=m CONFIG_NFT_LOG=m CONFIG_NFT_LIMIT=m CONFIG_NFT_MASQ=m CONFIG_NFT_REDIR=m CONFIG_NFT_NAT=m CONFIG_NFT_OBJREF=m CONFIG_NFT_REJECT=m CONFIG_NFT_COMPAT=m CONFIG_NFT_HASH=m CONFIG_NFT_DUP_NETDEV=m CONFIG_NFT_FWD_NETDEV=m CONFIG_NETFILTER_XT_TARGET_CONNMARK=m CONFIG_NETFILTER_XT_TARGET_CT=m CONFIG_NETFILTER_XT_TARGET_LED=m CONFIG_NETFILTER_XT_TARGET_LOG=m CONFIG_NETFILTER_XT_TARGET_MARK=m CONFIG_NETFILTER_XT_MATCH_ADDRTYPE=m CONFIG_NETFILTER_XT_MATCH_COMMENT=m CONFIG_NETFILTER_XT_MATCH_CONNBYTES=m CONFIG_NETFILTER_XT_MATCH_CONNLABEL=m CONFIG_NETFILTER_XT_MATCH_CONNLIMIT=m CONFIG_NETFILTER_XT_MATCH_CONNMARK=m CONFIG_NETFILTER_XT_MATCH_CONNTRACK=m CONFIG_NETFILTER_XT_MATCH_CPU=m CONFIG_NETFILTER_XT_MATCH_IPRANGE=m # CONFIG_NETFILTER_XT_MATCH_L2TP is not set CONFIG_NETFILTER_XT_MATCH_LENGTH=m CONFIG_NETFILTER_XT_MATCH_LIMIT=m CONFIG_NETFILTER_XT_MATCH_MAC=m CONFIG_NETFILTER_XT_MATCH_MARK=m CONFIG_NETFILTER_XT_MATCH_MULTIPORT=m CONFIG_NETFILTER_XT_MATCH_OWNER=m CONFIG_NETFILTER_XT_MATCH_PKTTYPE=m CONFIG_NETFILTER_XT_MATCH_RECENT=m CONFIG_NETFILTER_XT_MATCH_SOCKET=m CONFIG_NETFILTER_XT_MATCH_STATE=m CONFIG_NETFILTER_XT_MATCH_STATISTIC=m CONFIG_NETFILTER_XT_MATCH_TIME=m CONFIG_IP_SET=m CONFIG_IP_SET_BITMAP_IP=m CONFIG_IP_SET_BITMAP_IPMAC=m CONFIG_IP_SET_BITMAP_PORT=m CONFIG_IP_SET_HASH_IP=m CONFIG_IP_SET_HASH_IPMARK=m CONFIG_IP_SET_HASH_IPPORT=m CONFIG_IP_SET_HASH_IPPORTIP=m CONFIG_IP_SET_HASH_IPPORTNET=m CONFIG_IP_SET_HASH_MAC=m CONFIG_IP_SET_HASH_NETPORTNET=m CONFIG_IP_SET_HASH_NET=m CONFIG_IP_SET_HASH_NETNET=m CONFIG_IP_SET_HASH_NETPORT=m CONFIG_IP_SET_HASH_NETIFACE=m CONFIG_IP_SET_LIST_SET=m CONFIG_IP_NF_IPTABLES=m CONFIG_IP_NF_MATCH_RPFILTER=m CONFIG_IP_NF_MATCH_TTL=m CONFIG_IP_NF_FILTER=m CONFIG_IP_NF_TARGET_REJECT=m CONFIG_IP_NF_TARGET_SYNPROXY=m CONFIG_IP_NF_NAT=m CONFIG_IP_NF_TARGET_MASQUERADE=m CONFIG_IP_NF_TARGET_NETMAP=m CONFIG_IP_NF_TARGET_REDIRECT=m CONFIG_IP_NF_MANGLE=m CONFIG_IP_NF_TARGET_TTL=m CONFIG_IP_NF_RAW=m CONFIG_IP_NF_SECURITY=m CONFIG_IP6_NF_IPTABLES=m CONFIG_IP6_NF_MATCH_FRAG=m CONFIG_IP6_NF_MATCH_RPFILTER=m CONFIG_IP6_NF_FILTER=m CONFIG_IP6_NF_TARGET_REJECT=m CONFIG_IP6_NF_TARGET_SYNPROXY=m CONFIG_IP6_NF_MANGLE=m CONFIG_IP6_NF_RAW=m CONFIG_IP6_NF_SECURITY=m CONFIG_IP6_NF_NAT=m CONFIG_IP6_NF_TARGET_MASQUERADE=m CONFIG_IP6_NF_TARGET_NPT=m CONFIG_L2TP=m CONFIG_VLAN_8021Q=m CONFIG_VLAN_8021Q_GVRP=y CONFIG_NETLINK_DIAG=m CONFIG_BPF_JIT=y CONFIG_CAN=m CONFIG_CAN_C_CAN=m CONFIG_CAN_C_CAN_PLATFORM=m CONFIG_BT=m CONFIG_BT_RFCOMM=m CONFIG_BT_RFCOMM_TTY=y CONFIG_BT_BNEP=m CONFIG_BT_BNEP_MC_FILTER=y CONFIG_BT_BNEP_PROTO_FILTER=y CONFIG_BT_HIDP=m CONFIG_BT_HCIBTUSB=m CONFIG_BT_HCIBTSDIO=m CONFIG_BT_HCIUART=m CONFIG_BT_HCIUART_BCSP=y CONFIG_BT_HCIBCM203X=m CONFIG_BT_HCIBPA10X=m CONFIG_BT_HCIBFUSB=m CONFIG_BT_HCIVHCI=m CONFIG_BT_MRVL=m CONFIG_BT_MRVL_SDIO=m CONFIG_CFG80211=m CONFIG_MAC80211=m CONFIG_DEVTMPFS=y CONFIG_DEVTMPFS_MOUNT=y CONFIG_OMAP_OCP2SCP=y CONFIG_CONNECTOR=m CONFIG_MTD=y CONFIG_MTD_CMDLINE_PARTS=y CONFIG_MTD_BLOCK=y CONFIG_MTD_OOPS=y CONFIG_MTD_CFI=y CONFIG_MTD_CFI_INTELEXT=y CONFIG_MTD_PHYSMAP=y CONFIG_MTD_PHYSMAP_OF=y CONFIG_MTD_ONENAND=y CONFIG_MTD_ONENAND_VERIFY_WRITE=y CONFIG_MTD_ONENAND_OMAP2=y CONFIG_MTD_RAW_NAND=y CONFIG_MTD_NAND_OMAP2=y CONFIG_MTD_NAND_OMAP_BCH=y CONFIG_MTD_SPI_NOR=m CONFIG_MTD_UBI=y CONFIG_BLK_DEV_LOOP=y CONFIG_BLK_DEV_RAM=y CONFIG_BLK_DEV_RAM_SIZE=16384 CONFIG_SRAM=y CONFIG_EEPROM_AT24=m CONFIG_EEPROM_93CX6=y CONFIG_BLK_DEV_SD=y CONFIG_SCSI_SCAN_ASYNC=y CONFIG_ATA=y CONFIG_SATA_AHCI_PLATFORM=y CONFIG_NETDEVICES=y CONFIG_BONDING=m CONFIG_WIREGUARD=m CONFIG_MACVLAN=m CONFIG_MACVTAP=m CONFIG_IPVLAN=m CONFIG_IPVTAP=m CONFIG_VXLAN=m CONFIG_TUN=m # CONFIG_NET_VENDOR_ALACRITECH is not set # CONFIG_NET_VENDOR_AMAZON is not set # CONFIG_NET_VENDOR_AQUANTIA is not set # CONFIG_NET_VENDOR_ARC is not set # CONFIG_NET_VENDOR_AURORA is not set # CONFIG_NET_VENDOR_BROADCOM is not set # CONFIG_NET_VENDOR_CADENCE is not set # CONFIG_NET_VENDOR_CAVIUM is not set # CONFIG_NET_VENDOR_CIRRUS is not set # CONFIG_NET_VENDOR_CORTINA is not set # CONFIG_NET_VENDOR_EZCHIP is not set # CONFIG_NET_VENDOR_FARADAY is not set # CONFIG_NET_VENDOR_GOOGLE is not set # CONFIG_NET_VENDOR_HISILICON is not set # CONFIG_NET_VENDOR_HUAWEI is not set # CONFIG_NET_VENDOR_INTEL is not set # CONFIG_NET_VENDOR_MARVELL is not set # CONFIG_NET_VENDOR_MELLANOX is not set # CONFIG_NET_VENDOR_MICREL is not set # CONFIG_NET_VENDOR_MICROCHIP is not set # CONFIG_NET_VENDOR_MICROSEMI is not set # CONFIG_NET_VENDOR_NATSEMI is not set # CONFIG_NET_VENDOR_NETRONOME is not set # CONFIG_NET_VENDOR_NI is not set # CONFIG_NET_VENDOR_PENSANDO is not set # CONFIG_NET_VENDOR_QUALCOMM is not set # CONFIG_NET_VENDOR_RENESAS is not set # CONFIG_NET_VENDOR_ROCKER is not set # CONFIG_NET_VENDOR_SAMSUNG is not set # CONFIG_NET_VENDOR_SEEQ is not set # CONFIG_NET_VENDOR_SOLARFLARE is not set CONFIG_SMC91X=y CONFIG_SMC911X=y CONFIG_SMSC911X=y # CONFIG_NET_VENDOR_SOCIONEXT is not set # CONFIG_NET_VENDOR_STMICRO is not set # CONFIG_NET_VENDOR_SYNOPSYS is not set CONFIG_TI_DAVINCI_EMAC=y CONFIG_TI_CPSW=y # CONFIG_NET_VENDOR_VIA is not set # CONFIG_NET_VENDOR_WIZNET is not set # CONFIG_NET_VENDOR_XILINX is not set CONFIG_LED_TRIGGER_PHY=y CONFIG_MICROCHIP_T1_PHY=y CONFIG_SMSC_PHY=y CONFIG_USB_USBNET=m CONFIG_USB_NET_SMSC75XX=m CONFIG_USB_NET_SMSC95XX=m # CONFIG_USB_NET_NET1080 is not set # CONFIG_USB_NET_CDC_SUBSET is not set # CONFIG_USB_NET_ZAURUS is not set # CONFIG_WLAN_VENDOR_ADMTEK is not set # CONFIG_WLAN_VENDOR_ATH is not set # CONFIG_WLAN_VENDOR_ATMEL is not set # CONFIG_WLAN_VENDOR_BROADCOM is not set # CONFIG_WLAN_VENDOR_CISCO is not set # CONFIG_WLAN_VENDOR_INTEL is not set # CONFIG_WLAN_VENDOR_INTERSIL is not set # CONFIG_WLAN_VENDOR_MARVELL is not set # CONFIG_WLAN_VENDOR_MEDIATEK is not set # CONFIG_WLAN_VENDOR_MICROCHIP is not set # CONFIG_WLAN_VENDOR_RALINK is not set # CONFIG_WLAN_VENDOR_REALTEK is not set # CONFIG_WLAN_VENDOR_RSI is not set # CONFIG_WLAN_VENDOR_ST is not set # CONFIG_WLAN_VENDOR_TI is not set # CONFIG_WLAN_VENDOR_ZYDAS is not set # CONFIG_WLAN_VENDOR_QUANTENNA is not set CONFIG_INPUT_LEDS=m CONFIG_INPUT_POLLDEV=m CONFIG_INPUT_EVDEV=m CONFIG_KEYBOARD_ATKBD=m CONFIG_KEYBOARD_GPIO=m CONFIG_KEYBOARD_MATRIX=m CONFIG_KEYBOARD_OMAP4=m CONFIG_KEYBOARD_TWL4030=m # CONFIG_INPUT_MOUSE is not set CONFIG_INPUT_TOUCHSCREEN=y CONFIG_TOUCHSCREEN_ADS7846=m CONFIG_TOUCHSCREEN_EDT_FT5X06=m CONFIG_TOUCHSCREEN_TI_AM335X_TSC=m CONFIG_TOUCHSCREEN_PIXCIR=m CONFIG_TOUCHSCREEN_TSC2005=m CONFIG_TOUCHSCREEN_TSC2007=m CONFIG_INPUT_MISC=y CONFIG_INPUT_TPS65218_PWRBUTTON=m CONFIG_INPUT_TWL4030_PWRBUTTON=m CONFIG_INPUT_PALMAS_PWRBUTTON=m CONFIG_SERIO=m CONFIG_VT_HW_CONSOLE_BINDING=y # CONFIG_LEGACY_PTYS is not set CONFIG_SERIAL_8250=y CONFIG_SERIAL_8250_CONSOLE=y CONFIG_SERIAL_8250_NR_UARTS=32 CONFIG_SERIAL_8250_EXTENDED=y CONFIG_SERIAL_8250_MANY_PORTS=y CONFIG_SERIAL_8250_SHARE_IRQ=y CONFIG_SERIAL_8250_DETECT_IRQ=y CONFIG_SERIAL_8250_RSA=y CONFIG_SERIAL_8250_OMAP=y CONFIG_SERIAL_OF_PLATFORM=y CONFIG_SERIAL_OMAP=y CONFIG_SERIAL_OMAP_CONSOLE=y CONFIG_HW_RANDOM=y CONFIG_I2C_CHARDEV=y CONFIG_SPI=y CONFIG_SPI_OMAP24XX=y CONFIG_SPI_TI_QSPI=m CONFIG_SPI_SPIDEV=m CONFIG_HSI=m CONFIG_OMAP_SSI=m CONFIG_PINCTRL_SINGLE=y CONFIG_DEBUG_GPIO=y CONFIG_GPIO_SYSFS=y CONFIG_GPIO_PCA953X=m CONFIG_GPIO_PCF857X=y CONFIG_GPIO_PALMAS=y CONFIG_GPIO_TWL4030=y CONFIG_POWER_RESET=y CONFIG_BATTERY_BQ27XXX=m CONFIG_CHARGER_ISP1704=m CONFIG_CHARGER_TWL4030=m CONFIG_CHARGER_BQ2415X=m CONFIG_CHARGER_BQ24190=m CONFIG_CHARGER_BQ24735=m CONFIG_SENSORS_GPIO_FAN=m CONFIG_SENSORS_LM75=m CONFIG_SENSORS_TMP102=m CONFIG_THERMAL_GOV_FAIR_SHARE=y CONFIG_THERMAL_GOV_USER_SPACE=y CONFIG_CPU_THERMAL=y CONFIG_TI_SOC_THERMAL=m CONFIG_TI_THERMAL=y CONFIG_OMAP3_THERMAL=y CONFIG_OMAP4_THERMAL=y CONFIG_OMAP5_THERMAL=y CONFIG_DRA752_THERMAL=y CONFIG_WATCHDOG=y CONFIG_WATCHDOG_NOWAYOUT=y CONFIG_OMAP_WATCHDOG=y CONFIG_TWL4030_WATCHDOG=y CONFIG_MFD_TI_AM335X_TSCADC=m CONFIG_MFD_PALMAS=y CONFIG_MFD_TPS65217=y CONFIG_MFD_TPS65218=y CONFIG_MFD_TPS65910=y CONFIG_MFD_TWL4030_AUDIO=y CONFIG_TWL6040_CORE=y CONFIG_REGULATOR_PALMAS=y CONFIG_REGULATOR_PBIAS=y CONFIG_REGULATOR_TI_ABB=y CONFIG_REGULATOR_TPS62360=m CONFIG_REGULATOR_TPS65023=y CONFIG_REGULATOR_TPS6507X=y CONFIG_REGULATOR_TPS65217=y CONFIG_REGULATOR_TPS65218=y CONFIG_REGULATOR_TPS65910=y CONFIG_REGULATOR_TWL4030=y CONFIG_HID_GENERIC=m CONFIG_USB_HIDDEV=y CONFIG_USB_KBD=m CONFIG_USB_MOUSE=m CONFIG_USB=m CONFIG_USB_ANNOUNCE_NEW_DEVICES=y CONFIG_USB_MON=m CONFIG_USB_XHCI_HCD=m CONFIG_USB_EHCI_HCD=m CONFIG_USB_OHCI_HCD=m CONFIG_USB_WDM=m CONFIG_USB_STORAGE=m CONFIG_USB_MUSB_HDRC=m CONFIG_USB_MUSB_DSPS=m CONFIG_USB_TI_CPPI41_DMA=y CONFIG_USB_DWC3=m CONFIG_USB_TEST=m CONFIG_USB_GADGET=m CONFIG_USB_GADGET_DEBUG=y CONFIG_USB_GADGET_DEBUG_FILES=y CONFIG_USB_CONFIGFS=m CONFIG_USB_CONFIGFS_SERIAL=y CONFIG_USB_CONFIGFS_ACM=y CONFIG_USB_CONFIGFS_OBEX=y CONFIG_USB_CONFIGFS_NCM=y CONFIG_USB_CONFIGFS_ECM=y CONFIG_USB_CONFIGFS_ECM_SUBSET=y CONFIG_USB_CONFIGFS_RNDIS=y CONFIG_USB_CONFIGFS_EEM=y CONFIG_USB_CONFIGFS_MASS_STORAGE=y CONFIG_USB_CONFIGFS_F_LB_SS=y CONFIG_USB_CONFIGFS_F_FS=y CONFIG_USB_CONFIGFS_F_HID=y CONFIG_USB_ZERO=m CONFIG_MMC=y CONFIG_SDIO_UART=y CONFIG_MMC_SDHCI=y CONFIG_MMC_SDHCI_PLTFM=y CONFIG_MMC_OMAP=y CONFIG_MMC_OMAP_HS=y CONFIG_MMC_SDHCI_OMAP=y CONFIG_NEW_LEDS=y CONFIG_LEDS_CLASS=y CONFIG_LEDS_GPIO=y CONFIG_LEDS_PWM=y CONFIG_LEDS_TRIGGERS=y CONFIG_LEDS_TRIGGER_TIMER=y CONFIG_LEDS_TRIGGER_ONESHOT=y CONFIG_LEDS_TRIGGER_HEARTBEAT=y CONFIG_LEDS_TRIGGER_BACKLIGHT=m CONFIG_LEDS_TRIGGER_CPU=y CONFIG_LEDS_TRIGGER_GPIO=y CONFIG_LEDS_TRIGGER_DEFAULT_ON=y CONFIG_LEDS_TRIGGER_TRANSIENT=y CONFIG_RTC_CLASS=y CONFIG_RTC_DRV_DS1307=m CONFIG_RTC_DRV_TWL92330=y CONFIG_RTC_DRV_TWL4030=m CONFIG_RTC_DRV_PALMAS=m CONFIG_RTC_DRV_OMAP=y CONFIG_DMADEVICES=y CONFIG_UIO=m CONFIG_UIO_PRUSS=m CONFIG_COMMON_CLK_PALMAS=m CONFIG_HWSPINLOCK=y CONFIG_HWSPINLOCK_OMAP=m CONFIG_MAILBOX=y CONFIG_OMAP2PLUS_MBOX=m # CONFIG_IOMMU_SUPPORT is not set CONFIG_REMOTEPROC=y CONFIG_WKUP_M3_RPROC=m CONFIG_SOC_TI=y CONFIG_WKUP_M3_IPC=m CONFIG_TI_PRUSS=m CONFIG_TI_EMIF=m CONFIG_IIO=m CONFIG_TI_AM335X_ADC=m CONFIG_PWM=y CONFIG_PWM_OMAP_DMTIMER=m CONFIG_PWM_TIECAP=m CONFIG_PWM_TIEHRPWM=m CONFIG_PWM_TWL=m CONFIG_PWM_TWL_LED=m CONFIG_TI_PRUSS_INTC=m CONFIG_PHY_DM816X_USB=m CONFIG_OMAP_USB2=m CONFIG_TI_PIPE3=y CONFIG_EXT2_FS=y CONFIG_EXT3_FS=y CONFIG_FANOTIFY=y CONFIG_QUOTA=y CONFIG_QFMT_V2=y CONFIG_AUTOFS4_FS=m CONFIG_OVERLAY_FS=y CONFIG_MSDOS_FS=y CONFIG_VFAT_FS=y CONFIG_TMPFS=y CONFIG_TMPFS_POSIX_ACL=y CONFIG_CONFIGFS_FS=y CONFIG_JFFS2_FS=y CONFIG_JFFS2_SUMMARY=y CONFIG_JFFS2_FS_XATTR=y CONFIG_JFFS2_COMPRESSION_OPTIONS=y CONFIG_JFFS2_LZO=y CONFIG_JFFS2_RUBIN=y CONFIG_UBIFS_FS=y CONFIG_NFS_FS=y CONFIG_NFS_V3_ACL=y CONFIG_NFS_V4=y CONFIG_ROOT_NFS=y CONFIG_NLS_CODEPAGE_437=y CONFIG_NLS_ISO8859_1=y CONFIG_SECURITY=y CONFIG_CRYPTO_DH=m CONFIG_CRYPTO_ECRDSA=m CONFIG_CRYPTO_CURVE25519=m CONFIG_CRYPTO_CHACHA20POLY1305=m CONFIG_CRYPTO_AEGIS128=m CONFIG_CRYPTO_SEQIV=m CONFIG_CRYPTO_ECHAINIV=m CONFIG_CRYPTO_CTS=m CONFIG_CRYPTO_PCBC=m CONFIG_CRYPTO_CRC32=m CONFIG_CRYPTO_MICHAEL_MIC=y CONFIG_CRYPTO_AES_TI=m CONFIG_CRYPTO_BLOWFISH=m CONFIG_CRYPTO_DES=m CONFIG_CRYPTO_FCRYPT=m CONFIG_CRYPTO_LZ4=m CONFIG_CRYPTO_DEV_OMAP=m CONFIG_CRYPTO_DEV_OMAP_SHAM=m CONFIG_CRYPTO_DEV_OMAP_AES=m CONFIG_CRYPTO_DEV_OMAP_DES=m CONFIG_CRC_CCITT=y CONFIG_CRC_T10DIF=y CONFIG_CRC_ITU_T=y CONFIG_CRC7=y CONFIG_LIBCRC32C=y CONFIG_DMA_CMA=y CONFIG_PRINTK_TIME=y # CONFIG_DEBUG_BUGVERBOSE is not set CONFIG_DEBUG_INFO=y CONFIG_MAGIC_SYSRQ=y CONFIG_SCHEDSTATS=y CONFIG_PROVE_LOCKING=y