This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM62X: ping command fails with static ip

Part Number: PROCESSOR-SDK-AM62X
Other Parts Discussed in Thread: SK-AM62

Hello TI,

using SK-AM62 EVM board to connect with PC directly, set static ipaddr and serverip, the EVM fails to ping serverip.

  • Hi,

    I am able to ping another machine on my EVM from u-boot. I did use a static IP but I did not use the 169.254.x.x address range though. So I would recommend trying the EVM on a network that has a dhcp router to confirm that the EVM can send/receive in u-boot. Then I would recommend verifying the traffic between the EVM and that the PC is receiving packets by using wireshark. 

    Best Regards,

    Schuyler