This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI TVP5146/47 decoder driver

Other Parts Discussed in Thread: AM3517, TVP5146

Hi,

I'm writing to request your help, once again ! :D

I have to recompile linux kernel for the AM3517 processor, with the sdk 04.02.00.07. There are two different drivers for TVP5146/47 decoder, one based on sub-dev framework (tvp514x.c) and the other based on v4l2 framework (tvp514x-int.c), as stated here:

http://e2e.ti.com/support/embedded/f/354/t/56169.aspx

Since I performed kernel compilation even with sdk 03.00.00.02, I have noticed that previously there were files named tvp514x.c and tvp514-sd.c.

Was tvp514x-sd.c based on v4l2 framework and tvp514x on sub-dev ? If so, could you explain  me why its suffix changed from "-sd" to "-int" ?

 

Thanks in advance,

daniele